Issue
Define what Network 8000 devices that can be integrated with EcoStruxure Building Operation.
Product Line
EcoStruxure Building Operation, TAC I/A Series
Environment
- EcoStruxure Building Operation Automation Server version 1.2 until and including 3.2
- Network 8000
Cause
Need to know the supported devices for a Network 8000 to EcoStruxure Building Operation upgrade.
Resolution
EcoStruxure Building Operation supports the following Network 8000 LCM devices:
- LCM
EcoStruxure Building Operation supports the following Network 8000 ASD devices:
- Microzone II
- MicroFlo II
- LIM
- PEM
The following Micronet 2000 products are supported:
- MN-FLO
- MN-FLO3T
- MN-HPFC
- MN-ASDI
The following Network 8000 products are not supported in EcoStruxure Building Operation:
- CCL GCM
- LNC
- SIM GCM
- PLC
Note: EcoStruxure Building Operation version 4.0 (EBO 2022) and higher are not supported