APC UPS Data Center & Enterprise Solutions Forum
Schneider, APC support forum to share knowledge about installation and configuration for Data Center and Business Power UPSs, Accessories, Software, Services.
Posted: 2021-07-01 01:07 AM
This was originally posted on APC forums on 2/10/2012
I have installed vMA 5 on an ESXi 5 host. I installed PCNS 3 with the patch that replaced the install_en.sh and added the uninstall.
To test to make sure the machine will shut down. I use the vMA console and go to:
/opt/APC/PowerChute/group1/bin/ and run sudo ./shutdown.pl
I get:
Can't load '/usr/lib/perl5/site_perl/5.10.0/libvmatargetlib_perl.so' for module vmatargetlib_perl: libtypes.so: cannot open shared object file: No such file or directory at /usr/lib/perl5/5.10.0/x86_64-linux-thread-multi/DynaLoader.pm line 203.
at /usr/lib/perl5/site_perl/5.10.0/VMware/VmaTargetLib.pm line 10.
Compilation failed in require at /usr/lib/perl5/site_perl/5.10.0/VMware/VIFPLib.pm line 9.
BEGIN failed--compilation aborted at /usr/lib/perl5/site_perl/5.10.0/VMware/VIFPLib.pm line 9.
Compilation failed in require at ./shutdownhost.pl line 17.
BEGIN failed--compilation aborted at ./shutdownhost.pl line 17.
My next problem is I can't get to the web ui of the host, which I believe is a firewall issue and will tackle that once I know the PCNS is working.
Thanks for any help!
-Steve
Posted: 2021-07-01 01:07 AM
This reply was originally posted by Angela on APC forums on 1/8/2013
how to do this is in the knowledge base. search for FA159765 in http://www.apc.com/site/support/index.cfm/faq/ and refer to the section titled: How to verify communication ports are open in the vMA and how to add host servers to the server list
Posted: 2021-07-01 01:07 AM
This was originally posted on APC forums on 2/10/2012
Thanks for writing, I saw that article and had replaced the files before the install.
Posted: 2021-07-01 01:07 AM
This reply was originally posted by Angela on APC forums on 2/10/2012
i wonder if you are having this issue?
http://nam-en.apc.com/app/answers/detail/a_id/11500
Posted: 2021-07-01 01:07 AM
This reply was originally posted by Bill on APC forums on 2/13/2012
To verify PCNS is running run the command
sudo /etc/init.d/PowerChute status
If PCNS is running the system will return “PowerChute is running…”
If it is not running you can start it by typing
sudo /etc/init.d/PowerChute start
To test shutdown
1. CD to /opt/APC/PowerChute/group1 dir
2. run sudo bin/shutdown
Posted: 2021-07-01 01:07 AM
This was originally posted on APC forums on 2/13/2012
Thanks for that! I got "PowerChute is running..."
Then I used the shutdown command you gave and it shutdown the host!
When I turned the host back on, I went to the logs of one of the VMs (Server 2008). It says that the previous shutdown was unexpected. Shouldn't the host shutdown the VMs first?
Posted: 2021-07-01 01:07 AM
This was originally posted on APC forums on 2/13/2012
OK, thanks again to "i picKed a winna" and this link:
Linkie
I clicked over to this link: Linkie
And configured my automatic shutdown from there...
On my 2 Windows VMs, I altered the poweroff-vm-default.bat file and added "shutdown /s /f" to the end of the file and saved. Then when I did the "bin/shutdown" command it gracefully shutdown the VMs...
Still working on the web ui...
Message was edited by: forced
Posted: 2021-07-01 01:07 AM
This was originally posted on APC forums on 2/13/2012
My next issue is with the web ui for the vm host. I disabled the firewall, and got a "Internet Explorer cannot display the webpage".
I added the attached apc.xml file to the /etc/vmware/firewall folder. Then I refreshed by using "esxcli network firewall refresh". When I go the security profile screen of the vm host using the vsphere client, I can see the APC id listed and it is checked. I tried the web ui again but got the same result.
the apc.xml file is:
Posted: 2021-07-01 01:07 AM
This was originally posted on APC forums on 3/5/2012
force,
can you provide the details you used to fix the problem. i am having the same issues with vm's not being gracefully shutdown. I, as you, referenced the link that 'wanna' referenced.
my host shuts down but the vms hard power off.
Posted: 2021-07-01 01:07 AM
This reply was originally posted by Angela on APC forums on 3/6/2012
i edited the other posters post to retrieve this link for you: http://kb.vmware.com/selfservice/microsites/search.do?language=en_US&cmd=displayKC&externalId=100818...
Posted: 2021-07-01 01:07 AM
This was originally posted on APC forums on 1/8/2013
Hi !
How to check or change APC FIREWALL SETTING ?
Thank you !
Posted: 2021-07-01 01:07 AM
This was originally posted on APC forums on 1/8/2013
Hi,
the link given not working, i got a same issue cannot access ui web,
maybe firewall issue.
Thank you
Posted: 2021-07-01 01:07 AM
This reply was originally posted by Angela on APC forums on 1/8/2013
how to do this is in the knowledge base. search for FA159765 in http://www.apc.com/site/support/index.cfm/faq/ and refer to the section titled: How to verify communication ports are open in the vMA and how to add host servers to the server list
Create your free account or log in to subscribe to the forum - and gain access to more than 10,000+ support articles along with insights from experts and peers.