Ask our Experts
Didn't find what you are looking for? Ask our experts!
Share Your Feedback – Help Us Improve Search on Community! Please take a few minutes to participate in our Search Feedback Survey. Your insights will help us deliver the results you need faster and more accurately. Click here to take the survey
Get support to configure, troubleshoot, update or upgrade your motor management solution built with Altivar variable speed drives and Tesys devices to start, control, protect and monitor Low Voltage and Medium Voltage motors and loads, covering direct start, soft start and variable speed control.
Search in
Link copied. Please paste this link to share this article on your social media post.
Posted: 2022-10-21 08:43 AM . Last Modified: 2023-06-09 02:54 AM
What is the difference between the motor control type SVC I and SVC V in ATV71?
When do I need to select SVC I ?
Link copied. Please paste this link to share this article on your social media post.
Link copied. Please paste this link to share this article on your social media post.
Posted: 2024-11-05 09:50 AM
SVC U and SVC I are both open loop vector control . U fluxed by voltage and I fluxed by current.
SVC U we can say that is the standard vector control with slip compensation , compatible for single and parallel motors( identical motors) . Autotune is mandatory to have good performance , but motor model inside is more flexible and less rigid.
SVC I it is used when high performance control is needed with single motor ( not possible to be used with motor in parallel ) , Motor model is adjusted more carefully during autotune , optimizing the motor parameters=> basically we have a better motor model inside the drive => better control , it used for application like winder unwinder (torque control) , cranes , high speed or when high dynamic response is needed.
Link copied. Please paste this link to share this article on your social media post.
Link copied. Please paste this link to share this article on your social media post.
Posted: 2022-10-25 12:39 AM
I always wondered the same thing. I think manual said something like SVC I is equal to the behaviour of the older ATV58 drives. But it does not say exactly what this "behaviour" is. As they decided to keep this "legacy" mode it has to have some positive effects too on some loads but I guess it's usage is probably very limited as SVC V was chosen as default.
Link copied. Please paste this link to share this article on your social media post.
Link copied. Please paste this link to share this article on your social media post.
Posted: 2024-04-27 05:20 AM
svci is used when you have high demand load with fluctuation, if the motor doesn't have encoder feedback the vfd will manage the current to keep the motor in working as much possible in the optimum current and torque based on motor standard specs . while svcv is only used to keep frequency and voltage control of simple applications like fans , conveyors , ...
Link copied. Please paste this link to share this article on your social media post.
Link copied. Please paste this link to share this article on your social media post.
Posted: 2024-05-01 03:05 AM
Sounds like you are referring SVC U like a scalar mode but it is not, both are vector modes. But you might be right that SVC I has advantages in demanding applications. The manual that not say anything about that, only that SVC I mimics the behaviour of older ATV58 drives.
Link copied. Please paste this link to share this article on your social media post.
Link copied. Please paste this link to share this article on your social media post.
Posted: 2024-11-05 09:50 AM
SVC U and SVC I are both open loop vector control . U fluxed by voltage and I fluxed by current.
SVC U we can say that is the standard vector control with slip compensation , compatible for single and parallel motors( identical motors) . Autotune is mandatory to have good performance , but motor model inside is more flexible and less rigid.
SVC I it is used when high performance control is needed with single motor ( not possible to be used with motor in parallel ) , Motor model is adjusted more carefully during autotune , optimizing the motor parameters=> basically we have a better motor model inside the drive => better control , it used for application like winder unwinder (torque control) , cranes , high speed or when high dynamic response is needed.
Link copied. Please paste this link to share this article on your social media post.
Link copied. Please paste this link to share this article on your social media post.
Posted: 2024-11-05 11:44 PM
svc- i uses current control and this is good for fluctuating loads
svc- v uses voltage control which is good for torque and frequency precise control of loads
in general voltage control for general loads is better , in heavy equipment current is better .
Link copied. Please paste this link to share this article on your social media post.
Link copied. Please paste this link to share this article on your social media post.
Posted: 2024-11-13 12:01 AM
Interesting! I thought all kinds of vector control required single motor installations. But for me it doesn't matter much anyway since I dislike doing multi motors on a single VSD anyway 🙂 But I'm a bit curious on how the modern modells (320/600/900) hadle the SVC U/I choice since I think the option is now gone, is it SVC U only now?
Link copied. Please paste this link to share this article on your social media post.
You’ve reached the end of your document
Create your free account or log in to subscribe to the board - and gain access to more than 10,000+ support articles along with insights from experts and peers.