Posted: 2024-01-04 07:23 AM
Just bought starter kit and so far looks good apart from Edit Schedules
Using my Android phone Galaxy S10e
I can select and Edit Schedule
Edit Event
Temperature :I can change
When : I can change the start time
However I can see how to set the end time.
Am I doing something relay odd (properly)
App version 6.6.0
- Labels:
-
Apps
- Tags:
- english
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
Posted: 2024-04-03 07:01 AM
the end time is determined by the start time of the next event. So unless your house is really cold....
the following would give you heating on at 0900 off at 1100 back on at 1400 and off at 2300.
it does take a little bit of getting your head around but once you've done it a couple of times it becomes obvious.
Start 09:00 19°
Start 11:00 13°
Start 14:00 20°
Start 23:00 13°
(Hub 2, 15 TRV's, 2 rooms stats and 3 extenders)
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
Posted: 2024-04-03 07:01 AM
the end time is determined by the start time of the next event. So unless your house is really cold....
the following would give you heating on at 0900 off at 1100 back on at 1400 and off at 2300.
it does take a little bit of getting your head around but once you've done it a couple of times it becomes obvious.
Start 09:00 19°
Start 11:00 13°
Start 14:00 20°
Start 23:00 13°
(Hub 2, 15 TRV's, 2 rooms stats and 3 extenders)
Link copied. Please paste this link to share this article on your social media post.