Please take a few minutes to participate in our Search Feedback Survey. Your insights will help us deliver the results you need faster and more accurately.
Click here to take the survey

RemoteConnect Set Value from OBJ_WriteField

Remote Operations Forum

Support forum for Schneider Electric SCADA systems, radios and RTUs. From commissioning integration devices and software, to enhancing existing installations or troubleshooting.​
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
  • Remote Operations
  • Remote Operations Forum
  • RemoteConnect Set Value from OBJ_WriteField
Options
  • Mark Topic as New
  • Mark Topic as Read
  • Float this Topic for Current User
  • Bookmark
  • Subscribe
  • Mute
  • Printer Friendly Page
Invite a Co-worker
Send a co-worker an invite to the portal.Just enter their email address and we'll connect them to register. After joining, they will belong to the same company.
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
Joel_Weder
Captain Joel_Weder Captain
92
BevanWeiss
Spock BevanWeiss
24
sbeadle
Kirk sbeadle Kirk
17
View All

Recommended Forums

  • EcoStruxure Geo SCADA Expert Forum

  • APC UPS Data Center & Enterprise Solutions Forum

Invite a Colleague

Found this content useful? Share it with a Colleague!

Invite a Colleague Invite
Solved Go to Solution
Back to Remote Operations Forum
Start a Topic
Solved
tyler.knaup
Crewman tyler.knaup Crewman
Crewman

Posted: ‎2024-06-14 05:15 AM

0 Likes
4
1569
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
Posted: ‎2024-06-14 05:15 AM

RemoteConnect Set Value from OBJ_WriteField

Hello,

 

I was trying to set the .VALUE attribute of a RemoteConnect object using the OBJ_WriteField function. The help manual goes over the ATTRIB and DATATYPE fields for a system object, but it does not say that it works for a user defined object. Attempting to use the system fields results in a STATUS code of 5, or "Invalid attribute for the system function".

 

Is it possible to write to the .VALUE attribute through the code?

I am looking to use this to pull tagnames and default values from a CSV file to set the initial value of hundreds of tags when a default program is loaded.

Attachments
Labels
  • Labels:
  • RTU
  • Tags:
  • english
  • scada
  • SCADA app
  • SCADA software
  • SCADA tutorial
  • Telemetry and SCADA
Reply

Link copied. Please paste this link to share this article on your social media post.

  • All forum topics
  • Previous Topic
  • Next Topic

Accepted Solutions
Joel_Weder
Captain Joel_Weder Captain
Captain

Posted: ‎2024-06-20 11:16 AM

0 Likes
1
1478
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
Posted: ‎2024-06-20 11:16 AM

I've tested this and I believe I can see your issue. You've specified a DATATYPE of 2, which is only for System Data. It does require the data type be INT as you used, but that type is really only for system data. I set up the logic the same as yours and got the same status code 5. 

 

I changed the DATATYPE to 4 and changed the input object to a DINT in RemoteConnect. After that it is now working properly.  Unless you actually want to work with system data objects, look in the "Attribute constants for analog objects" table in the OBJ_WriteField help.

 

You can write to ValueRaw as a DINT (115) or ValueEng as a REAL (116), or to any of the other attributes of a T_SPx70 object.

 

 

Joel Weder
Remote Operations Specialist
Schneider Electric

See Answer In Context

Reply

Link copied. Please paste this link to share this article on your social media post.

Replies 4
vdsvds
Ensign vdsvds
Ensign

Posted: ‎2024-06-17 02:07 PM

0 Likes
0
1515
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
Posted: ‎2024-06-17 02:07 PM

Hi,

Did you consider using a structured text routine with direct value assignments? e.g.:

 

test_INT.VALUE := 1234;

test_INT2.VALUE := 5678;

Reply

Link copied. Please paste this link to share this article on your social media post.

tyler.knaup
Crewman tyler.knaup Crewman
Crewman

Posted: ‎2024-06-18 06:08 AM

0 Likes
0
1501
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
Posted: ‎2024-06-18 06:08 AM

I was trying to avoid hard coding any variables or values, as a master spreadsheet with DNP Point names/numbers and initial values creates a configuration csv to load in the scadapack. I am able to read the csv file with initial value currently, but I cannot find a way to set that value directly.

Reply

Link copied. Please paste this link to share this article on your social media post.

Joel_Weder
Captain Joel_Weder Captain
Captain

Posted: ‎2024-06-20 11:16 AM

0 Likes
1
1479
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
Posted: ‎2024-06-20 11:16 AM

I've tested this and I believe I can see your issue. You've specified a DATATYPE of 2, which is only for System Data. It does require the data type be INT as you used, but that type is really only for system data. I set up the logic the same as yours and got the same status code 5. 

 

I changed the DATATYPE to 4 and changed the input object to a DINT in RemoteConnect. After that it is now working properly.  Unless you actually want to work with system data objects, look in the "Attribute constants for analog objects" table in the OBJ_WriteField help.

 

You can write to ValueRaw as a DINT (115) or ValueEng as a REAL (116), or to any of the other attributes of a T_SPx70 object.

 

 

Joel Weder
Remote Operations Specialist
Schneider Electric
Reply

Link copied. Please paste this link to share this article on your social media post.

tyler.knaup
Crewman tyler.knaup Crewman
Crewman

Posted: ‎2024-06-20 12:54 PM

In response to Joel_Weder
0 Likes
0
1469
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
Posted: ‎2024-06-20 12:54 PM

Thank you.

 

I saw that this is now fully supported, and slightly better documented in RemoteConnect R3.0.5 that was just released, and am able to find the correct enumerations of the ATTRIB and DATATYPE parameters now.
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
Create your free account or log in to subscribe to the board - and gain access to more than 10,000+ support articles along with insights from experts and peers.