Our Community ranking system has recently been updated. You may notice changes in user rankings and receive system messages or notifications. If you have questions about how the new ranking works, please refer to the announcement post for more details (click here).

Remote Operations Forum

Support forum for Schneider Electric SCADA systems, radios and RTUs. From commissioning integration devices and software, to enhancing existing installations or troubleshooting.​
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
  • Remote Operations
  • Remote Operations Forum
  • Label: RTU
Options
  • Mark all as New
  • Mark all as Read
  • Float this item to the top
  • Subscribe
  • Bookmark
  • Invite a Friend
Invite a Co-worker
Send a co-worker an invite to the portal.Just enter their email address and we'll connect them to register. After joining, they will belong to the same company.
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
Label: "rtu"

View in: "Remote Operations Forum" | Community

155 Posts | First Used: 2019-10-25

Top Labels
Top Labels
  • Alphabetical
  • RTU 155
  • SCADA 139
  • Radio 120
  • Telemetry 85
  • Logic 45
  • DNP3 44
  • IAN (Instrument Area Network) 20
  • IoT 17
  • Drivers 14
  • ViewX 11
  • Scripting 7
  • Virtual ViewX 6
  • WITS 5
  • Redundancy 5
  • Battery life 4
  • WebX 3
  • Mimics 3
  • Trends 2
  • Smart Operations 1
  • Batch 1
  • Calculation 1
  • Ideas of improvements 1
  • SCADAPack 1
  • Realflo Flow 1
  • Smart Design & Engineering 1
  • Previous
  • 1 of 3
  • Next

Invite a Colleague

Found this content useful? Share it with a Colleague!

Invite a Colleague Invite

Remote Operations Forum

  • « Previous
    • 1
    • 2
    • 3
    • …
    • 15
  • Next »
  • All
  • Solved
  • Unsolved
  • Unanswered
Informational
Jimi
Jimi Troubleshooter

Geo SCADA Information

Here is a list of useful links related to Geo SCADA, all in one post. Please note, some of these links may change, if you see one that has stopped working, please reply to this post and I'll update it....
Remote Operations icon_circle Remote Operations Forum
267 0 0

2026-01-22

Informational
Jimi
Jimi Troubleshooter

Trio Data Radios Information

Here is a list of useful links related to Trio Radios, all in one post. Please note, some of these links may change, if you see one that has stopped working, please reply to this post and I'll update i...
Remote Operations icon_circle Remote Operations Forum
244 1 0

2026-01-22

Informational
Jimi
Jimi Troubleshooter

SCADAPack Information

Here is a list of useful links related to SCADAPack RTU's, all in one post. Please note, some of these links may change, if you see one that has stopped working, please reply to this post and I'll upda...
Remote Operations icon_circle Remote Operations Forum
316 0 0

2026-01-22

Solved
AlexNolan
AlexNolan

Modbus Communications to a Scadapack 474

I have a SCADAPack 474 sitting on my desk. It's set up with a fairly simple program including a number of Modbus AO points (DNPAO_200, Modbus DINT 40400/40401) these points exist as modbus read/write t...
Remote Operations icon_circle Remote Operations Forum
85 0 2
Latest Reply: AlexNolan

Solved
uguratak
uguratak

SCADAPack RemoteConnect - RuntimeFrame.NativeUtilities.dll Error & Per...

Hi everyone, I am experiencing a persistent crash with SCADAPack RemoteConnect on a laptop running Windows 11 24H2, while the same setup works perfectly on another laptop running 23H2. The Problem: The...
Remote Operations icon_circle Remote Operations Forum
313 0 2
Latest Reply: Joel_Weder

Informational
Jimi
Jimi Troubleshooter

SCADAPack Information

Here is a list of useful links related to SCADAPack RTU's, all in one post. Please note, some of these links may change, if you see one that has stopped working, please reply to this post and I'll upda...
Remote Operations icon_circle Remote Operations Forum
316 0 0

2026-01-22

Solved
jouharn
jouharn Contributor

ScadaPack 570 Communication issue

We are experiencing an issue at site where the Scada Pack 570 RTU communication with the SCADA station does not restore automatically after the telecom switch reboots. The RTU and SCADA station are on ...
Remote Operations icon_circle Remote Operations Forum
1521 0 6
Latest Reply: jouharn

Solved
rlao
rlao

Zero Threshold Limits for analog readings with both negative and posit...

Is there a way to set up Zero Threshold Limits for analog readings that have a negative minimum? For example, bidirectional flowmeters can log both reverse and forward flows on a -x L/s to +x L/s range...
Remote Operations icon_circle Remote Operations Forum
550 0 1
Latest Reply: Joel_Weder

Solved
mhis
mhis

Easy Logic EM6436H shows Comm Err F in DIAG screen

I am trying to connect my EasyLogic EM6436H to ION setup through RS485. But every time ION shows no response and meter Diagnostics screen shows Comm Err F. I google for the error code and found illegal...
Remote Operations icon_circle Remote Operations Forum
683 0 1
Latest Reply: Joel_Weder

Solved
geoffpatton
geoffpatton

SCADAPack 6606 Input Output module can not change the Configurable Dig...

I am programming for a SCADAPack 474 that will be installed with a 6606 module. I have added the module in RemoteConnect and for the Configurable Digital Input/Outputs will not let me change them from ...
Remote Operations icon_circle Remote Operations Forum
1299 0 3
Latest Reply: Joel_Weder

Solved
Scadapack474
Scadapack474

Question about DNP3 Configuration in Scadapack474

Hi, I am working on a project with Scadapack474 and VTScada where I am using DNP3, there is an option in remoteconnect under the basic tab in the object editor which says periodic event generation. If ...
Remote Operations icon_circle Remote Operations Forum
1493 0 3
Latest Reply: TTurner

Solved
shahaa
shahaa

Hi helo using telepace studio 5.4.2 with scadapack32, in that need tod...

how to access GPS data
Remote Operations icon_circle Remote Operations Forum
613 0 1
Latest Reply: Joel_Weder

Solved
Teaan
Teaan

Elementary Function Not Available Remote Connect

Hi, I am using Schneider Electric's General Purpose Libraries for an M580 application. I know need to implement SCADAPack 474's onsite for remote monitoring. Part of the libraries requires the use of...
Remote Operations icon_circle Remote Operations Forum
658 0 1
Latest Reply: Joel_Weder

Solved
TTurner
TTurner

Remote Connect 3.2.2 x70 474 Scadapack. Dumps Logic editor. Watchdog e...

We have a wellsite running a SP 474. Remote connect vers. 3.2.2. Firmware is 9.10.2.11300. Keeps dumping the logic editor program on software task watchdog. Code 0x0200. We have an almost identical ...
Remote Operations icon_circle Remote Operations Forum
1006 0 1
Latest Reply: Joel_Weder

  • « Previous
    • 1
    • 2
    • 3
    • …
    • 15
  • Next »
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
Create your free account or log in to subscribe to the board - and gain access to more than 10,000+ support articles along with insights from experts and peers.