Please take a few minutes to participate in our Search Feedback Survey. Your insights will help us deliver the results you need faster and more accurately.
Click here to take the survey

Polling Realflo Registers into RemoteConnect Logic Editor

Remote Operations Forum

Support forum for Schneider Electric SCADA systems, radios and RTUs. From commissioning integration devices and software, to enhancing existing installations or troubleshooting.​
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
  • Remote Operations
  • Remote Operations Forum
  • Polling Realflo Registers into RemoteConnect Logic Editor
Options
  • Mark Topic as New
  • Mark Topic as Read
  • Float this Topic for Current User
  • Bookmark
  • Subscribe
  • Mute
  • Printer Friendly Page
Invite a Co-worker
Send a co-worker an invite to the portal.Just enter their email address and we'll connect them to register. After joining, they will belong to the same company.
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
Joel_Weder
Captain Joel_Weder Captain
92
BevanWeiss
Spock BevanWeiss
24
sbeadle
Kirk sbeadle Kirk
17
View All

Recommended Forums

  • EcoStruxure Geo SCADA Expert Forum

  • APC UPS Data Center & Enterprise Solutions Forum

Invite a Colleague

Found this content useful? Share it with a Colleague!

Invite a Colleague Invite
Solved Go to Solution
Back to Remote Operations Forum
Start a Topic
Solved
Joel_Weder
Captain Joel_Weder Captain
Captain

Posted: ‎2022-12-14 09:30 AM . Last Modified: ‎2022-12-14 09:43 AM

1 Like
2
1678
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
Posted: ‎2022-12-14 09:30 AM . Last Modified: ‎2022-12-14 09:43 AM

Polling Realflo Registers into RemoteConnect Logic Editor

There are currently two ways to get Realflo data into RemoteConnect and the Logic Editor within the same RTU. First, I’ll discuss configuring a Modbus Scanner in RemoteConnect. Then I will discuss how to use DFB's (derived function blocks). Typically, the Modbus Scanner method is preferred if many registers are to be polled, or if 6-digit Modbus registers must be polled. The DFB method may be preferable when only a few registers are to be polled, or if you are comfortable editing a DFB.

 

Using Modbus Scanner to Poll Reaflo Values
- While Offline, right-click on SCADAPack x70 Controller Settings -DeviceDTM
- Select Additional Functions, then Project Settings. This is where you’ll have enabled Realflo.
- Enable the Modbus IP Client, allowing the RTU to perform IP polling, then click OK to close this dialog.
- In the Modbus configuration area, you’ll now see the Client item. Select this.
- Click the Add Device button. Give the new Client a name e.g. “Realflo Polling”
- Enter an IP address of 127.0.0.1 (the "localhost" or same RTU that Realflo is on)
- Click OK, then Apply the change
- Expand Client by clicking the [+] and select the client just created
- Click the Add Scanners button
- Set the Modbus Data Type to Real (or as required), then enter the required register address 
- Enter the required Register Quantity (remember, two registers per Real) then click OK
- Select Automatically Create and Connect new Objects then click OK and Apply
- The new objects are assigned names such as MBUS_Realflo_REAL_4xxxx. You can change these to something more meaningful, such as Run1_FlowRate.
- Configure the new objects with appropriate Logic Variable Type e.g. T_SPx70_ADV_ANALOG.
- The objects may now be used in Logic Editor.

 

Using DFB's to Poll, GET or SET Realflo Registers
If you need to make use of flow run instantaneous values, or change/view Realflo configuration values, several DFB's (derived function blocks) have been provided in the "x70 Logic Function Blocks" sub-folder under Program Files (x86) > Schneider Electric > Realflo. The needed DFB may be imported into Logic Editor, then used to get the value from Realflo. One additional DFB not included in that folder is attached to this post, which may be used to poll the flow computer for a Float value.

 

- In Logic Editor, right-click on Derived FB Types and select Import 

- Navigate to Program Files (x86) > Schneider Electric > Realflo > x70 Logic Function Blocks. (or to wherever you saved the "getregfloat" DFB) and select the desired DFB

- Once the DFB has been imported, you may right-click on it to Put in Library for later use as well

- Next, create a logic section and in the FFB Input Assistant simply create an instance of the DFB

 

NOTES about the getregfloat DFB:

- If desired to poll more than one Float (Real), simply daisy-chain two or more instances. Tie the Done output of the first to the Request input of the next.

- This DFB is only able to work with 5-digit Modbus registers, not 6-digit

 

Joel Weder
Remote Operations Specialist
Schneider Electric
Attachments
getregfloat5.zip
Labels
  • Labels:
  • RTU
  • SCADA
  • Telemetry
  • Tags:
  • english
  • Flow Computer
  • Realflo
  • scada
  • SCADA app
  • SCADA software
  • SCADA tutorial
  • Telemetry and SCADA
Reply

Link copied. Please paste this link to share this article on your social media post.

  • All forum topics
  • Previous Topic
  • Next Topic

Accepted Solutions
Joel_Weder
Captain Joel_Weder Captain
Captain

Posted: ‎2024-07-26 10:08 PM

In response to tturner45
0 Likes
0
956
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
Posted: ‎2024-07-26 10:08 PM

There's actually a newer version now, version 6. And yes it's certainly possible to poll regularly.

 

Joel Weder
Remote Operations Specialist
Schneider Electric

See Answer In Context

Attachments
GetRegFloatv6.zip
Reply

Link copied. Please paste this link to share this article on your social media post.

Replies 2
tturner45
tturner45
Cadet

Posted: ‎2024-07-25 10:09 AM

0 Likes
1
958
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
Posted: ‎2024-07-25 10:09 AM

Hi Joel, 

In older versions I remember you couldn't constantly poll Realflo and Read/Write to Realflo without getting errors. Is that still the case? This block is perfect for an application I'm building where I don't need to create a scanner every time. I still want my Realflo to be functional if I poll every scan or once every second or something.

Thanks.

 

Reply

Link copied. Please paste this link to share this article on your social media post.

Joel_Weder
Captain Joel_Weder Captain
Captain

Posted: ‎2024-07-26 10:08 PM

In response to tturner45
0 Likes
0
957
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
Posted: ‎2024-07-26 10:08 PM

There's actually a newer version now, version 6. And yes it's certainly possible to poll regularly.

 

Joel Weder
Remote Operations Specialist
Schneider Electric
Attachments
GetRegFloatv6.zip
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
Create your free account or log in to subscribe to the board - and gain access to more than 10,000+ support articles along with insights from experts and peers.