Please take a few minutes to participate in our Search Feedback Survey. Your insights will help us deliver the results you need faster and more accurately.
Click here to take the survey

PowerLogic T300 - When used as a slave IEC 104 device of ABB RTU, why is analog data reading slow?

Protection & Control

Schneider Electric support forum about Protection Relays, Substation Controllers & RTUs, Arc Flash Devices & Systems in Medium Voltage and Low Voltage. A place to get support on product selection, installation, commissioning and troubleshooting.
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
  • EcoStruxure Power & Grid
  • Protection & Control
  • PowerLogic T300 - When used as a slave IEC 104 device of ABB RTU, why is analog data reading slow?
Options
  • Mark Topic as New
  • Mark Topic as Read
  • Float this Topic for Current User
  • Bookmark
  • Subscribe
  • Mute
  • Printer Friendly Page
Invite a Co-worker
Send a co-worker an invite to the portal.Just enter their email address and we'll connect them to register. After joining, they will belong to the same company.
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
Araceli_Monje
Commander Araceli_Monje Commander
43
Arun-kumar_PS
Commander Arun-kumar_PS Commander
21
View All

Recommended Forums

  • Metering & Power Quality

  • SmartConnector Forum

Invite a Colleague

Found this content useful? Share it with a Colleague!

Invite a Colleague Invite
Solved Go to Solution
Back to Protection & Control
Start a Topic
Solved
Hoang_Phu
Ensign Hoang_Phu
Ensign

Posted: ‎2025-03-28 02:27 AM . Last Modified: ‎2025-05-16 12:16 AM

2 Likes
3
927
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
‎2025-03-28 02:27 AM

PowerLogic T300 - When used as a slave IEC 104 device of ABB RTU, why is analog data reading slow?

Hello guys, good day. I have a question for you all. I am reading the analog data of P5 relay from T300 rtu and sending it to ABB rtu via 104 protocol, but the value I am sending is being read very slowly on ABB rtu, maybe changing after 3-5 minutes. The digital value is fine. The analog value that T300 is reading is normal. What settings have I missed?

Labels
  • Labels:
  • Application cases
  • PowerLogic P3
  • PowerLogic P5
  • PowerLogic T300
Tags (5)
  • Tags:
  • english
  • IEC 104
  • p3
  • P5
  • t300
Reply
  • All forum topics
  • Previous Topic
  • Next Topic

Accepted Solutions
Mathieu_Lansoy
Lt. Commander Mathieu_Lansoy Lt. Commander
Lt. Commander

Posted: ‎2025-05-15 03:04 AM

1 Like
0
843
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
‎2025-05-15 03:04 AM

Hello,

 

The transmission of analogue values using IEC 104 Protocol is linked to different processes:

- the client (here ABB RTU) is sending a "General Interrogation" request to the server (T300). The server will answer with the content of all its IEc104 database (including analogue values). (this can also be done with a specific "read" request to read only some variables). (the period for this request is a setting of the client)

- cyclic analogue events: some elements of the database can also be sent cyclically by the T300 (T300 IEC104 settings. here for example, all "MMEC" variables will be sent cyclicly every 120s)

Mathieu_Lansoy_0-1747302017899.png

 

- spontaneous  events: if a "Threshold" is associated to a analogue variable, a spontaneous event (that can be timestamped) is generated when the gap with the last sent value is higher than the thresold, and sent to the client. The threshold is expressed in absolute value (not in percentage).

Here a threshold of 10(A) is associated to the Phase current, so each time the variation of the current (versus the last sent value) will be higher than 10 A, an event will be transmitted.

Mathieu_Lansoy_0-1747302582949.png

Typically, we are using 10(A) for currents, 1000 (or 1500)(V) for (MV) voltages, 10000 for powers, 5(°) for temperature. But it can be adapted to have more or less events.

 

We don't have the configuration for this project, we can suppose that thresholds are not set on the T300, and cyclic scan neither. So the refresh of analogue values on the client is only due to GI rate. (3 min ?)

Advice: set some thresholds to the analogues values that are shared with the ABB RTU.

(this is done in Easergy Builder / coreDb : Analog tab / Destinationx Threshold)

 

Regards,

 

  Mathieu.

 

 

See Answer In Context

Reply
Replies 3
Araceli_Monje
Commander Araceli_Monje Commander
Commander

Posted: ‎2025-05-15 02:23 AM

0 Likes
0
847
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
‎2025-05-15 02:23 AM

@Mathieu_Lansoy , hi, could you please support with this question?, thx.

Reply
Mathieu_Lansoy
Lt. Commander Mathieu_Lansoy Lt. Commander
Lt. Commander

Posted: ‎2025-05-15 03:04 AM

1 Like
0
844
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
‎2025-05-15 03:04 AM

Hello,

 

The transmission of analogue values using IEC 104 Protocol is linked to different processes:

- the client (here ABB RTU) is sending a "General Interrogation" request to the server (T300). The server will answer with the content of all its IEc104 database (including analogue values). (this can also be done with a specific "read" request to read only some variables). (the period for this request is a setting of the client)

- cyclic analogue events: some elements of the database can also be sent cyclically by the T300 (T300 IEC104 settings. here for example, all "MMEC" variables will be sent cyclicly every 120s)

Mathieu_Lansoy_0-1747302017899.png

 

- spontaneous  events: if a "Threshold" is associated to a analogue variable, a spontaneous event (that can be timestamped) is generated when the gap with the last sent value is higher than the thresold, and sent to the client. The threshold is expressed in absolute value (not in percentage).

Here a threshold of 10(A) is associated to the Phase current, so each time the variation of the current (versus the last sent value) will be higher than 10 A, an event will be transmitted.

Mathieu_Lansoy_0-1747302582949.png

Typically, we are using 10(A) for currents, 1000 (or 1500)(V) for (MV) voltages, 10000 for powers, 5(°) for temperature. But it can be adapted to have more or less events.

 

We don't have the configuration for this project, we can suppose that thresholds are not set on the T300, and cyclic scan neither. So the refresh of analogue values on the client is only due to GI rate. (3 min ?)

Advice: set some thresholds to the analogues values that are shared with the ABB RTU.

(this is done in Easergy Builder / coreDb : Analog tab / Destinationx Threshold)

 

Regards,

 

  Mathieu.

 

 

Reply
JYPOC
Commander JYPOC Commander
Commander

Posted: ‎2025-05-16 12:22 AM . Last Modified: ‎2025-05-16 12:24 AM

0 Likes
0
812
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
‎2025-05-16 12:22 AM

Hello @Hoang_Phu 

Your guess was correct, the issue you meet is solved by setting IEC 104 parameters accordingly.

As indicated by Mathieu, you can either do it on the ABB RTU (make a faster general interrogation) or change settings on T300: which one have you chosen?

Once you have implemented it and verified all is well, please mark Mathieu's proposal as a solution.

Regards

BR - Jean-Yves
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
Create your free account or log in to subscribe to the board - and gain access to more than 10,000+ support articles along with insights from experts and peers.