Protection & Control

Schneider Electric support forum about Protection Relays, Substation Controllers & RTUs, Arc Flash Devices & Systems in Medium Voltage and Low Voltage. A place to get support on product selection, installation, commissioning and troubleshooting.
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
  • EcoStruxure Power & Grid
  • Protection & Control
  • Label: PowerLogic T300
Options
  • Mark all as New
  • Mark all as Read
  • Float this item to the top
  • Subscribe
  • Bookmark
  • Invite a Friend
Invite a Co-worker
Send a co-worker an invite to the portal.Just enter their email address and we'll connect them to register. After joining, they will belong to the same company.
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
Label: "powerlogic t300"

View in: "Protection & Control" | Community

83 Posts | First Used: 2020-02-20

Top Labels
Top Labels
  • Alphabetical
  • Application cases 135
  • PowerLogic T300 83
  • PowerLogic P3 81
  • PowerLogic P5 56
  • MiCOM range 50
  • Training 41
  • Saitel range 40
  • IEC61850 31
  • Sepam range 16
  • PowerLogic P1 14
  • White Papers 14
  • PowerLogic T500 12
  • PowerLogic P7 9
  • Arc Flash 6
  • PowerTag Energy 2
  • Power Quality 1
  • IT Expert 1
  • Others & accessories 1
  • Previous
  • 1 of 2
  • Next

Invite a Colleague

Found this content useful? Share it with a Colleague!

Invite a Colleague Invite

Protection & Control

  • « Previous
    • 1
    • 2
    • 3
    • …
    • 8
  • Next »
  • All
  • Solved
  • Unsolved
  • Unanswered
Araceli_Monje
/html/rank_icons/Commander.png Araceli_Monje /html/rank_icons/SE-Employee.png

Welcome & Get Started to Protection & Control Forum!

Ready to discover our fully renewed Protection & Control portfolio? What is Protection & Control Forum about? This forum has been specifically designed to find support about: Protection...
EcoStruxure Power & Grid icon_circle Protection & Control
1196 1 0

2023-04-06

Solved
OdysseiaTiTi
/html/rank_icons/Crewman.png OdysseiaTiTi

PowerLogic T500 – TI=46 Double Command rejected; DO works only via web...

Hi all, I’m running an PowerLogic T500 (HU280 + DI180 + DO180) with Easergy Builder v1.7.49 as an IEC-104 slave (ASDU addr = 1, port 2404). What works Telemetry is fine: analogs and double-point DI...
EcoStruxure Power & Grid icon_circle Protection & Control
347 0 5
Latest Reply: JuanRayo

Solved
Hoang_Phu
/html/rank_icons/Ensign.png Hoang_Phu

I cannot control a circuit breaker using the Micom 30x relay output.

I want to ask something. I have been using IEC61850 for a while. I want to read the IEC61850 CID file with T300 Rtu and control the breaker remotely. But I can't configure the control. As I understand ...
EcoStruxure Power & Grid icon_circle Protection & Control
449 0 3
Latest Reply: Araceli_Monje

Solved
vietkhoatsi
vietkhoatsi

PowerLogic T300 - firmware upgrade from v1.4 to v2.7 and above

Hi All Im using T300 has Fw 1.4, i want update to 2.7 for using ATS feature, but it went wrong It must be upgrade from 1.4 to 1.5, 1.5 to 1.6, 1.6 to 2.7 So you guy can give file Fw 1.5, 1.6, .....
EcoStruxure Power & Grid icon_circle Protection & Control
1426 0 6
Latest Reply: THO_NGUYEN

Solved
Aimen_Abdelazim
/html/rank_icons/Ensign.png Aimen_Abdelazim /html/rank_icons/SE-Employee.png

Substation Automation webinars for Q4 2020

Eager to learn about the new features and applications already available in Digital Power offers and how they contribute to the value proposition and differentiation? Do not miss our webinars delivered...
EcoStruxure Power & Grid icon_circle Protection & Control
1208 1 2
Latest Reply: Ahmedabdelfatah

Solved
hweimann
/html/rank_icons/Crewman.png hweimann

T300 firmware

How can i obtain the new firmware of T300 HU250?
EcoStruxure Power & Grid icon_circle Protection & Control
359 0 2
Latest Reply: hweimann

Rile
Rile

Autorecloser in T300 FW 2.9.5

Hi, I have heard that latest version of SC160 should include autorecloser function. Anýone know if its true and have some experience of it? BR/risto
EcoStruxure Power & Grid icon_circle Protection & Control
463 0 1
Latest Reply: sathishkumar_ramakrishnan

Solved
jean-luc_batard
/html/rank_icons/Lieutenant_JG.png jean-luc_batard /html/rank_icons/SE-Employee.png

PowerLogic T300 - PS50 power supply, a key element for distribution au...

PS50 secure power supply is playing a real key role in PowerLogic T300 (formerly named Easergy T300) solution, as it ensures that the system is available at any time, especially when Mains power source...
EcoStruxure Power & Grid icon_circle Protection & Control
1308 2 4
Latest Reply: jean-luc_batard

Julio_CesarDguez
/html/rank_icons/Crewman.png Julio_CesarDguez /html/rank_icons/SE-Employee.png

Zone Selective Interlocking & T300

Hello Community!! Yesterday, a client contacted us with a question regarding the T300 included in the MV solution with RM AirSet panels, used for control and protection. Their inquiry concerns Zone Sel...
EcoStruxure Power & Grid icon_circle Protection & Control
265 0 1
Latest Reply: jean-luc_batard

Informational
Rajeev_211
/html/rank_icons/Crewman.png Rajeev_211 /html/rank_icons/SE-Employee.png

Easergy Builder - In CoreDB, how to configure Modbus slave device's SP...

Hi, I have to add a modbus slave device SPC (single point command) command having register address 1 (holding) HR bit 6 in Saitel HUe easergy builder configuration, how to map in coredb? I tried mapp...
EcoStruxure Power & Grid icon_circle Protection & Control
525 0 5
Latest Reply: JuanRayo

Solved
Hoang_Phu
/html/rank_icons/Ensign.png Hoang_Phu

PowerLogic T300 - Configuration to connect a "slave" IEC 61850 device

Hello engineers. I am new to HU250. If possible, please provide an example of adding a device to T300 using IEC 61850 protocol.
EcoStruxure Power & Grid icon_circle Protection & Control
794 0 3
Latest Reply: Hoang_Phu

Solved
Hoang_Phu
/html/rank_icons/Ensign.png Hoang_Phu

PowerLogic T300 - When used as a slave IEC 104 device of ABB RTU, why ...

Hello guys, good day. I have a question for you all. I am reading the analog data of P5 relay from T300 rtu and sending it to ABB rtu via 104 protocol, but the value I am sending is being read very slo...
EcoStruxure Power & Grid icon_circle Protection & Control
809 2 3
Latest Reply: JYPOC

  • « Previous
    • 1
    • 2
    • 3
    • …
    • 8
  • Next »
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
Create your free account or log in to subscribe to the board - and gain access to more than 10,000+ support articles along with insights from experts and peers.