Hi everyone,
I am migrating my Control Expert project into Process Expert 2023 by importing ZEF archive file into
the Control Expert topology , and i got errors indicating that RIO drop RCA 31210 which is configured as DhCP client no assigned to DHCP server , on the DHCP view it is not possible to drag and drop the modules to the M580 CPU WHICH SUPPOSED to be the server, and not possiblr to do this un the RCA module properties
, check attached photos
any help
thanks