Our Community ranking system has recently been updated. You may notice changes in user rankings and receive system messages or notifications. If you have questions about how the new ranking works, please refer to the announcement post for more details (click here).

can IONsetup be used to read/display harmonics up to the 50th ?

Metering & Power Quality

Schneider Electric support forum about Power Meters (ION, PowerTag, PowerLogic) and Power Quality from design, implementation to troubleshooting and more.
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
  • can IONsetup be used to read/display harmonics up to the 50th ?
Options
  • Mark Topic as New
  • Mark Topic as Read
  • Float this Topic for Current User
  • Bookmark
  • Subscribe
  • Mute
  • Printer Friendly Page
Invite a Co-worker
Send a co-worker an invite to the portal.Just enter their email address and we'll connect them to register. After joining, they will belong to the same company.
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
582
Mehran_Mehrnia
Mehran_Mehrnia Champion
216
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
sesa38559
sesa38559 Leader
Leader

Posted: ‎2017-05-17 09:32 AM . Last Modified: ‎2020-04-22 01:17 AM

0 Likes
1
1239
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
‎2017-05-17 09:32 AM

can IONsetup be used to read/display harmonics up to the 50th ?

Customer has no software and is asking to see/ record / display harmonics up to the 50th using M7650 on site.

 

Many thanks 🙂

Labels
  • Labels:
  • ION Setup
Reply
  • All forum topics
  • Previous Topic
  • Next Topic
Reply 1
Robert_Lee
Robert_Lee Champion
Champion

Posted: ‎2017-05-17 09:49 AM . Last Modified: ‎2022-10-18 10:24 PM

1 Like
0
1196
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
‎2017-05-17 09:49 AM

Yes, this can be done but requires someone to create a custom table viewer.

Follow the first 4 steps in the following procedure:

https://community.se.com/message/67466?commentID=67466#comment-67466

Then you would copy one of the standard table viewers instead (ex. Realtime.PML) and open it up in Notepad.

Decide on what type of layout you want to create and determine which handles you need to retrieve (this can be done by either using the Advanced ION module view and examining the ION handles for whatever reading you are wanting to display or getting a list of available ION handles for the firmware you have if available).

Each "cell" in the table view, will likely be of the form:

R#C#=Addr,Format,Decimals,Label

ex. R2C2=0x5803,0,3,Volts LN Avg

Simply replace the Addr shown with the ION handle for each output you wish to show:

ex. R2C2=0x5902,0,3,V1 HD 3

would show the V1 3rd Harmonic value for the V1 Harmonics module.

You would likely need to change R#C1 values to change the displayed label shown down the first column (the one for each cell is not shown and is just a placeholder comment presently) and possibly the R1C# entries to change the column headings across the top.
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
Create your free account or log in to subscribe to the board - and gain access to more than 10,000+ support articles along with insights from experts and peers.