Our Community ranking system has recently been updated. You may notice changes in user rankings and receive system messages or notifications. If you have questions about how the new ranking works, please refer to the announcement post for more details (click here).

What is the solution we can offer for PM5000 with Analog Output ?

Metering & Power Quality

Schneider Electric support forum about Power Meters (ION, PowerTag, PowerLogic) and Power Quality from design, implementation to troubleshooting and more.
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
  • EcoStruxure Power & Grid
  • Metering & Power Quality
  • What is the solution we can offer for PM5000 with Analog Output ?
Options
  • Mark Topic as New
  • Mark Topic as Read
  • Float this Topic for Current User
  • Bookmark
  • Subscribe
  • Mute
  • Printer Friendly Page
Invite a Co-worker
Send a co-worker an invite to the portal.Just enter their email address and we'll connect them to register. After joining, they will belong to the same company.
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
Charles_Murison
Charles_Murison Champion
566
Mehran_Mehrnia
Mehran_Mehrnia Champion
195
Ramasamy_N
Ramasamy_N Champion
115
View All

Recommended Forums

  • SmartConnector Forum

Invite a Colleague

Found this content useful? Share it with a Colleague!

Invite a Colleague Invite
Solved Go to Solution
Back to Metering & Power Quality
Start a Topic
Solved
Anonymous user
Not applicable

Posted: ‎2014-03-10 05:53 AM

0 Likes
6
2307
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
‎2014-03-10 05:53 AM

What is the solution we can offer for PM5000 with Analog Output ?

We are discussing with Cummins, for Energy Monitoring in Sync Panel...Application calls for KW & KWH input to Sync PLC and at the same time they need to give all parameters to Clients EMS or BMS. So for this can they use Analog Output from Meter for KW & KWH as input to PLC and RS485 or Ethernet connectivity from Meter to Client.

We have PM8M2222 with PM800....can it be used for above application ?

What alternate we can offer for above in PM5000 ?

Regards,

Chetan Dhake.

Tags (3)
  • Tags:
  • ai
  • analog
  • ao
Reply
  • All forum topics
  • Previous Topic
  • Next Topic

Accepted Solutions
Abdel
Abdel Troubleshooter
Troubleshooter

Posted: ‎2014-03-14 11:18 AM

0 Likes
1
2200
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
‎2014-03-14 11:18 AM

Hi chetan,

Yes you cab use the analog output from the

PM8M2222 to sync PLC , one register should be linked to one digital output.For PM5000, i am now in the train, i will look for a solution this evening!

Regards

See Answer In Context

Reply
Replies 6
Abdel
Abdel Troubleshooter
Troubleshooter

Posted: ‎2014-03-14 11:18 AM

0 Likes
1
2201
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
‎2014-03-14 11:18 AM

Hi chetan,

Yes you cab use the analog output from the

PM8M2222 to sync PLC , one register should be linked to one digital output.For PM5000, i am now in the train, i will look for a solution this evening!

Regards

Reply
Abdel
Abdel Troubleshooter
Troubleshooter

Posted: ‎2014-03-14 11:20 AM

0 Likes
0
2200
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
‎2014-03-14 11:20 AM

Sorry i meant analog output, and don' t forget max and min value. Your PLC should have an analog input 4-20ma

Reply
JamesAZZO
JamesAZZO
Leader

Posted: ‎2014-03-15 05:54 AM

0 Likes
2
2200
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
‎2014-03-15 05:54 AM

Not possible with PM5xxx - must wait for PM8000 I believe.

Reply
Abdel
Abdel Troubleshooter
Troubleshooter

Posted: ‎2014-03-15 06:41 AM

0 Likes
1
2200
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
‎2014-03-15 06:41 AM

Hi,

It is not possible with PM5000 at the moment!

Reply
Abdel
Abdel Troubleshooter
Troubleshooter

Posted: ‎2014-03-17 01:19 AM

0 Likes
0
2200
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
‎2014-03-17 01:19 AM

Would you update this thread as "answered", if you are satisfied with the reply?

 

Thank you.

Reply
Yut
Yut
Leader

Posted: ‎2014-07-18 02:46 AM

2 Likes
0
2201
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
‎2014-07-18 02:46 AM

kWh and kVARh are accumulated value they keep increase you cannot use the analog output 2-40 mA, instead the digital output must be use to send energy pulses to the PLC counter.
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
Create your free account or log in to subscribe to the board - and gain access to more than 10,000+ support articles along with insights from experts and peers.