Our Community ranking system has recently been updated. You may notice changes in user rankings and receive system messages or notifications. If you have questions about how the new ranking works, please refer to the announcement post for more details (click here).

What are the limitations of using PM8000 as a Modbus gateway

Metering & Power Quality

Schneider Electric support forum about Power Meters (ION, PowerTag, PowerLogic) and Power Quality from design, implementation to troubleshooting and more.
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
  • EcoStruxure Power & Grid
  • Metering & Power Quality
  • What are the limitations of using PM8000 as a Modbus gateway
Options
  • Mark Topic as New
  • Mark Topic as Read
  • Float this Topic for Current User
  • Bookmark
  • Subscribe
  • Mute
  • Printer Friendly Page
Invite a Co-worker
Send a co-worker an invite to the portal.Just enter their email address and we'll connect them to register. After joining, they will belong to the same company.
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
Charles_Murison
Charles_Murison Champion
566
Mehran_Mehrnia
Mehran_Mehrnia Champion
195
Ramasamy_N
Ramasamy_N Champion
115
View All

Recommended Forums

  • SmartConnector Forum

Invite a Colleague

Found this content useful? Share it with a Colleague!

Invite a Colleague Invite
Solved Go to Solution
Back to Metering & Power Quality
Start a Topic
Solved
Yarom
Yarom Troubleshooter
Troubleshooter

Posted: ‎2024-11-04 06:02 AM

0 Likes
6
1804
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
‎2024-11-04 06:02 AM

What are the limitations of using PM8000 as a Modbus gateway

Hello,

 

I know that we can use the PM8240 (any PM8000) as  Modbus RTU to TCP gateway.  The question is are there limitations? Cases that we should not use it so?

 

We have a TAPCON device for an MV Transformer that communicates through RS485. We thought of putting a PAS600 gateway. We have in the same panel a PM8240 so thought perhaps to use the gateway feature.

 

Any information would be appreciated.

 

Yarom

Labels
  • Labels:
  • PM8000
Tags (1)
  • Tags:
  • english
Reply
  • All forum topics
  • Previous Topic
  • Next Topic

Accepted Solutions
Mehran_Mehrnia
Mehran_Mehrnia Champion
Champion

Posted: ‎2024-11-04 11:29 AM

1 Like
1
1759
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
‎2024-11-04 11:29 AM

Hi @Yarom 

 

So, in brief, PAS600 is exclusively designed for communication applications and Gateway functionality. However, ION meters such as PM8000 are mainly designed for metering and energy management applications, where communication capabilities are additional features considered as low priority, especially when the meter is busy with metering tasks such as power quality, waveform, and high-speed data recording.


When PM8000 is configured as a Gateway, it does not affect the TCP/IP network, and there should not be any limited number of registers, as it forwards the message to the serial devices or forwards the response back to the Modbus client, provided that the meter is not busy. Otherwise, it could affect response time, or in the worst case, the communication gets dropped if the meter's CPU is fully loaded.

 

Best Regards,

-Mehran

L3 Expert Advanced metering

See Answer In Context

Reply
Replies 6
Mehran_Mehrnia
Mehran_Mehrnia Champion
Champion

Posted: ‎2024-11-04 07:47 AM . Last Modified: ‎2024-11-04 07:48 AM

1 Like
1
1790
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
‎2024-11-04 07:47 AM

Hi @Yarom 

 

As mentioned in PM8000 user guide:
There are two types of Ethernet gateways that you can configure on your meter:
• EtherGate: A single TCP connection communicates through the gateway meter to a serial network of devices.
• Modbus gateway: Up to a maximum of 32 Modbus client TCP connections communicate through the gateway meter to a serial network of Modbus devices.

Mehran_Mehrnia_0-1730735219677.png

 



Best Regards,

-Mehran

L3 Expert Advanced metering

Reply
Yarom
Yarom Troubleshooter
Troubleshooter

Posted: ‎2024-11-04 07:52 AM

0 Likes
0
1789
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
‎2024-11-04 07:52 AM

Hi Mehran,

 

Yes. This part I know about. That is one of the purposes we are thinking of using the PM8240 installed. What I am asking is if there is some limitation as to using the PM8000 as a gateway? Are there a limited number of registers that can be used? Would using it as a gateway affect the TCP/IP network?

 

Are there any communication limitations that would get us to consider the PAS600 as a proper gateway?

 

Best regards,

 

Yarom

Reply
Mehran_Mehrnia
Mehran_Mehrnia Champion
Champion

Posted: ‎2024-11-04 11:29 AM

1 Like
1
1760
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
‎2024-11-04 11:29 AM

Hi @Yarom 

 

So, in brief, PAS600 is exclusively designed for communication applications and Gateway functionality. However, ION meters such as PM8000 are mainly designed for metering and energy management applications, where communication capabilities are additional features considered as low priority, especially when the meter is busy with metering tasks such as power quality, waveform, and high-speed data recording.


When PM8000 is configured as a Gateway, it does not affect the TCP/IP network, and there should not be any limited number of registers, as it forwards the message to the serial devices or forwards the response back to the Modbus client, provided that the meter is not busy. Otherwise, it could affect response time, or in the worst case, the communication gets dropped if the meter's CPU is fully loaded.

 

Best Regards,

-Mehran

L3 Expert Advanced metering

Reply
Yarom
Yarom Troubleshooter
Troubleshooter

Posted: ‎2024-11-04 11:16 PM

0 Likes
0
1737
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
‎2024-11-04 11:16 PM

Thank you for that! That was what I was looking for and wanted to make sure.

 

Best regards.

Reply
dan2071
dan2071
Explorer

Posted: ‎2025-01-16 01:08 PM

0 Likes
0
1543
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
‎2025-01-16 01:08 PM

Could you tell me if it is possible to read the values of a PM8000 once it has been setup as a Modbus Master? I can see all RTU slaves through the PM8000 but not the actual PM8000.

 

I so, could you advise on how to add this into EBO.

 

Thanks, Dan

Reply
Mehran_Mehrnia
Mehran_Mehrnia Champion
Champion

Posted: ‎2025-01-17 08:43 AM

1 Like
0
1532
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
‎2025-01-17 08:43 AM

Hi @dan2071 

 

No matter whether the PM8000 is set up as a Modbus Master or Modbus Gateway, it can be polled by any Modbus client tool to provide the requested data by setting the slave ID of the PM8000 meter to 255 and using a Modbus access right of 'Read/Write' or 'Read Only.'

 

This forum is dedicated to Metering & Power Quality. To get assistance on EBO and how to add the device and registers, please post your question in EcoStruxure Building Operation Forum.

 

Best Regards,

-Mehran

L3 Expert Advanced metering
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
Create your free account or log in to subscribe to the board - and gain access to more than 10,000+ support articles along with insights from experts and peers.