Ask our Experts
Didn't find what you are looking for? Ask our experts!
New Community Ranking System
Our Community ranking system has recently been updated. You may notice changes in user rankings and receive system messages or notifications. If you have questions about how the new ranking works, please refer to the announcement post for more details (click here).
Schneider Electric support forum about Power Meters (ION, PowerTag, PowerLogic) and Power Quality from design, implementation to troubleshooting and more.
Search in
Please select a country to continue with beta search.
Link copied. Please paste this link to share this article on your social media post.
Hi,
I was wondering if it is possible to view the current value(s) in internal registers of a PM8000 through ION Setup.
For instance if I have an arithmetic block with two inputs(sources) and one output (result) is there a way to see what the current values of those inputs and output are?
I have attempted to use a custom display and browse for those registers but no compatible registers are found as per the attached screenshot.
Link copied. Please paste this link to share this article on your social media post.
Yes, here are two methods:
1. The method you chose works fine for me to show any output on a Display (up to 6 values per display, and the PM8000 now has up to 40 custom displays on v4.0.0).
Aha I see there was a known issue with older versions of ION Setup. https://www.se.com/ca/en/faqs/FA253222/
2. To temporarily see the values within the ION Setup Advanced Configuration, hold the shift button down on your keyboard when clicking on the Input and Output tab.
Link copied. Please paste this link to share this article on your social media post.
Yes, here are two methods:
1. The method you chose works fine for me to show any output on a Display (up to 6 values per display, and the PM8000 now has up to 40 custom displays on v4.0.0).
Aha I see there was a known issue with older versions of ION Setup. https://www.se.com/ca/en/faqs/FA253222/
2. To temporarily see the values within the ION Setup Advanced Configuration, hold the shift button down on your keyboard when clicking on the Input and Output tab.
Link copied. Please paste this link to share this article on your social media post.
Hi Dan,
Your second option works. On the first one however I am not sure what my issue is as I have ION Setup 3.2.23004.01 installed.
Firmware of the meter is as per the screenshot. I will attempt to upgrade the firmware to v4.0 which I see has just become available to see if this remedies the issue.
Thanks for the assistance.
Link copied. Please paste this link to share this article on your social media post.
You’ve reached the end of your document
Create your free account or log in to subscribe to the board - and gain access to more than 10,000+ support articles along with insights from experts and peers.