TCP Number of Connections PM8000, PM5000 and PM800 series

Metering & Power Quality

Schneider Electric support forum about Power Meters (ION, PowerTag, PowerLogic) and Power Quality from design, implementation to troubleshooting and more.
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
  • EcoStruxure Power & Grid
  • Metering & Power Quality
  • TCP Number of Connections PM8000, PM5000 and PM800 series
Options
  • Mark Topic as New
  • Mark Topic as Read
  • Float this Topic for Current User
  • Bookmark
  • Subscribe
  • Mute
  • Printer Friendly Page
Invite a Co-worker
Send a co-worker an invite to the portal.Just enter their email address and we'll connect them to register. After joining, they will belong to the same company.
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
Charles_Murison
Picard Charles_Murison Picard
525
Mehran_Mehrnia
Admiral Mehran_Mehrnia Admiral
138
Ramasamy_N
Captain Ramasamy_N Captain
115
View All

Recommended Forums

  • SmartConnector Forum

Invite a Colleague

Found this content useful? Share it with a Colleague!

Invite a Colleague Invite
Solved Go to Solution
Back to Metering & Power Quality
Start a Topic
Solved
sesa82206
sesa82206 Schneider Alumni (Retired)
Schneider Alumni (Retired)

Posted: ‎2015-08-18 08:54 AM

0 Likes
6
3215
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
‎2015-08-18 08:54 AM

TCP Number of Connections PM8000, PM5000 and PM800 series

Team,

What is the max number of simultaneous TCP connections a:

-  PM8xxx can support?

- PM5xxx ?

- PM8xx ?

Regards,

Tags (8)
  • Tags:
  • connection
  • pm5000
  • pm5xxx
  • pm800
  • pm8000
  • pm8xx
  • pmxxx
  • tcp
Reply
  • All forum topics
  • Previous Topic
  • Next Topic

Accepted Solutions
ram_kaushik
Admiral ram_kaushik Admiral
Admiral

Posted: ‎2015-08-18 10:00 AM

0 Likes
3
3095
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
‎2015-08-18 10:00 AM

Ivan - from the PM8000 specification - 32 concurrent TCP/IP connections. Still looking into PM5000 since it is not captured in the spec..

See Answer In Context

Reply
Replies 6
ram_kaushik
Admiral ram_kaushik Admiral
Admiral

Posted: ‎2015-08-18 10:00 AM

0 Likes
3
3096
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
‎2015-08-18 10:00 AM

Ivan - from the PM8000 specification - 32 concurrent TCP/IP connections. Still looking into PM5000 since it is not captured in the spec..

Reply
sesa56307_bridg
Lieutenant JG sesa56307_bridg Lieutenant JG
Lieutenant JG

Posted: ‎2015-08-18 02:54 PM

1 Like
2
3095
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
‎2015-08-18 02:54 PM

To be more specific, the 32 concurrent TCP/IP connections are dedicated to Modbus TCP (port 502), but a number of additional connections are also supported.

Here is a screenshot of a good summary from the PM8000 user manual:

7224

Reply
Usha
Commander Usha Commander
Commander

Posted: ‎2015-08-19 02:51 AM

1 Like
1
3095
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
‎2015-08-19 02:51 AM

For PM5300 class of meters have been tested to support up to 3 concurrent TCP connections.

For PM5500 class of meter support up to 32 concurrent TCP connections.


Regards,
Usha
Software Engineering Support
Reply
JamesAZZO
Sisko | EcoXpert Master JamesAZZO Sisko | EcoXpert Master
Sisko | EcoXpert Master

Posted: ‎2015-08-19 06:24 AM

0 Likes
1
3095
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
‎2015-08-19 06:24 AM

What is the difference between Modbus TCP and Modbus TCP (dedicated)?

Reply
sesa82206
sesa82206 Schneider Alumni (Retired)
Schneider Alumni (Retired)

Posted: ‎2015-08-19 06:40 AM

0 Likes
0
3095
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
‎2015-08-19 06:40 AM

Thank you Usha,

Are there any documents available tgat contain this onformation that I can share with customer? Specs doc, design guides, etc?

Reply
sesa64419
sesa64419 Schneider Alumni (Retired)
Schneider Alumni (Retired)

Posted: ‎2015-08-19 07:58 AM

2 Likes
0
3095
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
‎2015-08-19 07:58 AM

The PM8000 has 8 Ethernet connections that can be shared (used by) either ION, DNP or Modbus TCP or combination of all three.

There are also 32 Ethernet connections that can only be used by Modbus TCP.

So there are 32 dedicated (can only be used by) Modbus TCP connections, and there are up to 8 additional connections which could use Modbus TCP if desired (and you didn't want any ION or DNP connections).

I've heard some people call the 8 shared connections  "generic" connections as they can be used for either of the three protocols.

Modbus TCP is the only protocol that has both dedicated and shared connections, so they are differentiated in the table. The other protocols have dedicated connections (like IEC 61850).

Hope this helps.

Alana
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
Create your free account or log in to subscribe to the board - and gain access to more than 10,000+ support articles along with insights from experts and peers.