Ask our Experts
Didn't find what you are looking for? Ask our experts!
New Community Ranking System
Our Community ranking system has recently been updated. You may notice changes in user rankings and receive system messages or notifications. If you have questions about how the new ranking works, please refer to the announcement post for more details (click here).
Schneider Electric support forum about Power Meters (ION, PowerTag, PowerLogic) and Power Quality from design, implementation to troubleshooting and more.
Search in
Link copied. Please paste this link to share this article on your social media post.
Hi,
I would like to read recorded data from the ION 7410 device. I could not see any information about the reading recorded data in the documentation.
When I connected to device with FTP, there is a folder named logData. I believe that logData folder may have the data I want to read. But it seems like I have no permission to access the files in that folder. When I try to list the files inside that folder FTP server returns a response says 550 S_errno_EACCES. I'm connecting to the device with User1. Is there a user with required permissions for getting the files in logData folder?
Also I would appreciate any other method than FTP you can offer me for reading recorded data.
Thank you.
Link copied. Please paste this link to share this article on your social media post.
Hello @oguzyazan ,
The FTP folder logData does not have the information you are looking for. This folder is there for possible future features. To get the logged data I suggest you use the Tool ION Setup (ION Setup). With ION Setup you can use the Data view option to see the onboard logs.
Regards,
Charles
Link copied. Please paste this link to share this article on your social media post.
Hello @oguzyazan ,
The FTP folder logData does not have the information you are looking for. This folder is there for possible future features. To get the logged data I suggest you use the Tool ION Setup (ION Setup). With ION Setup you can use the Data view option to see the onboard logs.
Regards,
Charles
Link copied. Please paste this link to share this article on your social media post.
Hi,
I need to get logged data with my own software. So, ION Setup tool is not a solution for me. Is there a way to get logged data with a 3rd party software ?
Thanks.
Link copied. Please paste this link to share this article on your social media post.
Hello @oguzyazan ,
The only open protocol to get data log data at this time is DLMS. The ION protocol is propriety.
Regards,
Charles
Link copied. Please paste this link to share this article on your social media post.
Hi,
I tried to connect to the meter with DLMS protocol. I'm using Gurux DLMS library with .NET. I'm getting "Failed to receive reply from the device in given time" error. I think the problem may be the client or server address.
Settings that I used for connection:
Client address: 16
Server address: 1
Logical name referencing: yes
Interface type: HDLC
Protocol: TCP
Thanks.
Link copied. Please paste this link to share this article on your social media post.
Hello @oguzyazan
have a look at the post by Sanjeet at https://community.se.com/t5/Metering-Power-Quality/DLMS-over-Ethernet-test-client-software/m-p/15468.... Note Sanjeet's screenshot shows hex values.
Following is decimal information:
Client Address: 16
Logical server:1
Physical server: 100
Use Serial port through ethernet: Checked.
Depending on a number of setting on the device you may also need to increase the timeout settings. There are upcoming performance improvements to DLMS in a future firmware release of ION7400 meters.
As noted in previous post, if using Gurux library, it is best to use UTC time.
Regards,
Charles
You’ve reached the end of your document
Create your free account or log in to subscribe to the board - and gain access to more than 10,000+ support articles along with insights from experts and peers.