Send a co-worker an invite to the Exchange portal.Just enter their email address and we’ll connect them to register. After joining, they will belong to the same company.
Send Invite Cancel
84265members
353371posts

PowerTag F160 and Rope with FDM128

Metering & Power Quality

Collaborate with multiple experts and discuss various topics about Power Meters and Power Quality. From design & implementation to troubleshooting and more, get support from experts and share your experiences by subscribing to the Schneider Electric Exchange forum today.

Romain_Polette
Sisko Sisko
Sisko

PowerTag F160 and Rope with FDM128

Dear all, 

 

I want to inform you that PowerTag Energy F160 and Rope are now compatible with FDM128 using the same screens as PowerTag M250/M630.

 

To ensure this functionality up-grade, FDM128 needs to have its firmware updated :

https://www.se.com/ww/en/product/LV434128/ethernet-switchboard-display-fdm-128%2C-up-to-8-connected-...

 

Let me know if you have some questions.

Romain POLETTE - Solution architect - France Operation
Intencity - Grenoble - France
Tags (3)
3 Replies 3
Charles_Murison
Picard Picard
Picard
0 Likes
0
812

Re: PowerTag F160 and Rope with FDM128

Thank you for sharing.

 

Charles

 

L4 Prime for Advanced metering and Utilities
Tags (1)
Abigail-Lugo
Cadet
Cadet
0 Likes
1
604

Re: PowerTag F160 and Rope with FDM128

Romain_Polette 

 

thank you, is it the same for the 63A powertags?

Tags (1)
Romain_Polette
Sisko Sisko
Sisko
0 Likes
0
595

Re: PowerTag F160 and Rope with FDM128

Hello @Abigail-Lugo , 

Below the full list of sensors supported by FDM128 v8.0.25:

 

S.NO

Power Tags

NSX

F160

Rope

1

A9MEM1520

LV434020

A9MEM1580

A9MEM1590

2

A9MEM1521

LV434021

 

A9MEM1591

3

A9MEM1522

LV434022

 

A9MEM1592

4

A9MEM1540

LV434023

 

A9MEM1593

5

A9MEM1541

 

 

 

6

A9MEM1542

 

 

 

7

A9MEM1560

 

 

 

8

A9MEM1561

 

 

 

9

A9MEM1562

 

 

 

10

A9MEM1563

 

 

 

11

A9MEM1570

 

 

 

12

A9MEM1571

 

 

 

13

A9MEM1572

 

 

 

                                                                     To Be Supported

 

A9MEM1573

LVSMC13

 

 

 

A9MEM1574

LVSMC23

 

 

 

A9MEM1543

LVSMC14

 

 

 

A9MEM1564

LVSMC24

 

 

 

Regards, 

 

Romain POLETTE - Solution architect - France Operation
Intencity - Grenoble - France
Tags (1)