Schneider Electric support forum about Power Meters (ION, PowerTag, PowerLogic) and Power Quality from design, implementation to troubleshooting and more.
Send a co-worker an invite to the portal.Just enter their email address and we'll connect them to register. After joining, they will belong to the same company.
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
2024-04-0104:42 PM
PM8240 v4.5.0 network issue
Hi. We recently replaced some Dirius A30 meters with PM8240 meters. We have used the same IP address as the meter that was replaced. We are able to intermittently ping the meter, one ping will be received every 100 or so pings.
We also have PM8240 meters already in service. Comparing the configuration, there is no difference except the IP addresses.
The firmware of the new meter is v4.5.0. The old meters are v3.1.0.
Is there any known issues with network connections with v4.5.0? Otherwise any other reason for this issue?