Our Community ranking system has recently been updated. You may notice changes in user rankings and receive system messages or notifications. If you have questions about how the new ranking works, please refer to the announcement post for more details (click here).

PM8000V2 (fw v1.4.1) - ION over Modbus

Metering & Power Quality

Schneider Electric support forum about Power Meters (ION, PowerTag, PowerLogic) and Power Quality from design, implementation to troubleshooting and more.
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
  • PM8000V2 (fw v1.4.1) - ION over Modbus
Options
  • Mark Topic as New
  • Mark Topic as Read
  • Float this Topic for Current User
  • Bookmark
  • Subscribe
  • Mute
  • Printer Friendly Page
Invite a Co-worker
Send a co-worker an invite to the portal.Just enter their email address and we'll connect them to register. After joining, they will belong to the same company.
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
582
Mehran_Mehrnia
Mehran_Mehrnia Champion
216
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
Daniel_Brandao
Daniel_Brandao Mentor
Mentor

Posted: ‎2017-12-14 01:14 PM

3 Likes
2
1957
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
‎2017-12-14 01:14 PM

PM8000V2 (fw v1.4.1) - ION over Modbus

Hello everyone,

Another feature we are bringing with the new PM8000 v1.4.1 firmware is a new functionality called "ION over Modbus". This functionality was developed to facilitate PM8xx retrofit in serial networks. Below you can find the links for a short introductory presentation, a technical bulletin and a knowledge base article:

Presentation: PM8000 - ION over Modbus.pptx - Box

Technical bulletin: ION over Modbus communications for PM8000 and ION7400 series meters

kb article (=S= employees only): http://infocenter.schneider-electric.com/aps/index?page=home (search for ION over Modbus)

In order for the feature to work, PME needs to be updated with the latest cumulative update (CU1). Link can be found here: PME 8.2 CU1 - Box

Other features available with CU1:

  • Security hotfix for the Telerik component released in early November. Security Notification can be found HERE
  • Fix for SEPAM driver were under some circumstances a flood of events (Not Synchronous Status) are sent to the software.
  • VIP has been changed to prevent nuisance, duplicate alarms (setpoint modules) on VIP restart.

Thanks and let's attack our installed base!!

Tags (4)
  • Tags:
  • ion over modbus
  • pm8000
  • pm8xx
  • retrofit
Reply
  • All forum topics
  • Previous Topic
  • Next Topic
Replies 2
sesa108084_brid
sesa108084_brid Explorer
Explorer

Posted: ‎2018-06-28 09:33 AM

0 Likes
1
1861
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
‎2018-06-28 09:33 AM

Good day


Has anyone tested ION over Modbus with ION7650 and ION9000's gateway?

TQ
EY

Reply
Anonymous user
Not applicable

Posted: ‎2018-07-04 02:16 PM

1 Like
0
1862
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
‎2018-07-04 02:16 PM

Hello,

Yes IoM was tested using the ION7650 as the Modbus Gateway.

The implementation on the ION7650 of the Modbus TCP to Modbus RTU gateway has significant delays (500mS per frame) built in to prevent possible CPU overloading.  This results in compromised comm performance and slow performance when using IoM to a PM8000 due to the amount of data on the PM8000.  I would not recommend using the ION7650 as the Modbus gateway if it can be avoided.

Testing of the ION9000 (and PM8000) as a Modbus Gateway for IoM has been done and performance is the same as all the other Schneider Electric Gateways.

Jim
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
Create your free account or log in to subscribe to the board - and gain access to more than 10,000+ support articles along with insights from experts and peers.