Our Community ranking system has recently been updated. You may notice changes in user rankings and receive system messages or notifications. If you have questions about how the new ranking works, please refer to the announcement post for more details (click here).

PM8000 and Port 502

Metering & Power Quality

Schneider Electric support forum about Power Meters (ION, PowerTag, PowerLogic) and Power Quality from design, implementation to troubleshooting and more.
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
  • EcoStruxure Power & Grid
  • Metering & Power Quality
  • PM8000 and Port 502
Options
  • Mark Topic as New
  • Mark Topic as Read
  • Float this Topic for Current User
  • Bookmark
  • Subscribe
  • Mute
  • Printer Friendly Page
Invite a Co-worker
Send a co-worker an invite to the portal.Just enter their email address and we'll connect them to register. After joining, they will belong to the same company.
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
Charles_Murison
Charles_Murison Champion
566
Mehran_Mehrnia
Mehran_Mehrnia Champion
194
Ramasamy_N
Ramasamy_N Champion
115
View All

Recommended Forums

  • SmartConnector Forum

Invite a Colleague

Found this content useful? Share it with a Colleague!

Invite a Colleague Invite
Solved Go to Solution
Back to Metering & Power Quality
Start a Topic
Solved
michael_franz
michael_franz
Mentor

Posted: ‎2016-09-22 08:36 AM

0 Likes
4
2485
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
‎2016-09-22 08:36 AM

PM8000 and Port 502

We have four PM8000 meters in our lab.  Two of them will not except communication over Port 502.  The only obvious issue I can see is that the two that are not able to do Modbus coms have newer firmware.

All are being done over IP directly.  Each device has address 1.  All can be addressed with ION Setup and via their web page.

It may be a red herring but here is the list

Meter      Firmware          Readable

QED        001.003.001     No

DEMO     001.003.001     No

Meter      Firmware

MCC        001.002.014  Yes

Cart         001.000.057   Yes

The first two will not return register reads with Tester or a ComX 5100 The third and forth work with both.

Is there anything else we should check.  Should I back set them to older firmware.

Thanks,

Michael


Tags (3)
  • Tags:
  • 502
  • modbus
  • pm8000
Reply
  • All forum topics
  • Previous Topic
  • Next Topic

Accepted Solutions
Cliff_Schubert
Cliff_Schubert Troubleshooter
Troubleshooter

Posted: ‎2016-09-22 10:32 AM

2 Likes
2
2341
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
‎2016-09-22 10:32 AM

The 1.3.1 firmware fixed a a few Modbus & communications issues and also added IPv6 Support

(What's new here: PM8000 series firmware v1.3.1 what's new)

If port 502 is enabled as @Andrew Garbutt in the post above, are there any IPv6 settings in your environment that could be affecting things?

Does the meter communicate for a while but then stop?

See Answer In Context

Reply
Replies 4
Andrew_Garbutt
Andrew_Garbutt Leader
Leader

Posted: ‎2016-09-22 10:11 AM

1 Like
0
2340
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
‎2016-09-22 10:11 AM

Perhaps the protocol was disabled? For the PM8000, you can individually enable/disable various protocols from ION Setup, or through the Ethernet Comm module in Designer.

Setup Assistant.png

Reply
Cliff_Schubert
Cliff_Schubert Troubleshooter
Troubleshooter

Posted: ‎2016-09-22 10:32 AM

2 Likes
2
2342
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
‎2016-09-22 10:32 AM

The 1.3.1 firmware fixed a a few Modbus & communications issues and also added IPv6 Support

(What's new here: PM8000 series firmware v1.3.1 what's new)

If port 502 is enabled as @Andrew Garbutt in the post above, are there any IPv6 settings in your environment that could be affecting things?

Does the meter communicate for a while but then stop?

Reply
michael_franz
michael_franz
Mentor

Posted: ‎2016-09-22 11:45 AM

0 Likes
0
2340
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
‎2016-09-22 11:45 AM

Cliff:

Thanks, looks enabled.

502.png

Reply
michael_franz
michael_franz
Mentor

Posted: ‎2016-09-27 12:03 PM

1 Like
0
2340
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
‎2016-09-27 12:03 PM

fixed it
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
Create your free account or log in to subscribe to the board - and gain access to more than 10,000+ support articles along with insights from experts and peers.