Ask our Experts
Didn't find what you are looking for? Ask our experts!
New Community Ranking System
Our Community ranking system has recently been updated. You may notice changes in user rankings and receive system messages or notifications. If you have questions about how the new ranking works, please refer to the announcement post for more details (click here).
Schneider Electric support forum about Power Meters (ION, PowerTag, PowerLogic) and Power Quality from design, implementation to troubleshooting and more.
Search in
Please select a country to continue with beta search.
Link copied. Please paste this link to share this article on your social media post.
Bonjour,
une fois de plus j'ai un client (EDF) qui me demande de ne pas afficher les intensités en kA mais en A
la même chose pour la puissance, il me demande des kW, pas des MW.
J'ai trouvé une procédure pour créer un écran personnalisé qui affiche des A et des kW;
cela fonction très bien.
J'ai trouvé également une autre procédure pour modifier directement les pages de mesures de bases.
J'utilise IONSEtup mais dans le menu Display Modules j'ai une page vide à droite.
Je ne dois pas avoir le bon mot de passe.
Quelqu'un peut me le fournir?
Merci d'avance
Link copied. Please paste this link to share this article on your social media post.
Hello @Olivier_GARAULT ,
I am sorry I do not speak French but I believe the page can be translated. The meter comes with a number of displays defined in the firmware that do not require the display modules. The display modules are only for custom screens. To make the setting changes you are looking for the Display Option module. There is a setup register for display units.
Note that meter has auto scaling units be default based on CT primary setting. If CT primary > 1000, default units for current is kA. For example if your CT is 1200:5, rather than using CT primary = 1200 and CT secondary = 5, you can use CT primary = 240, and CT secondary = 1.
Voltage and power also have auto scaling, refer to user guide for more information.
Regards,
Charles
Link copied. Please paste this link to share this article on your social media post.
Hello @Olivier_GARAULT ,
I am sorry I do not speak French but I believe the page can be translated. The meter comes with a number of displays defined in the firmware that do not require the display modules. The display modules are only for custom screens. To make the setting changes you are looking for the Display Option module. There is a setup register for display units.
Note that meter has auto scaling units be default based on CT primary setting. If CT primary > 1000, default units for current is kA. For example if your CT is 1200:5, rather than using CT primary = 1200 and CT secondary = 5, you can use CT primary = 240, and CT secondary = 1.
Voltage and power also have auto scaling, refer to user guide for more information.
Regards,
Charles
Link copied. Please paste this link to share this article on your social media post.
Bonjour,
j'ai actuellement des CT 1000/1A et on ne comprend pas que les intensités soient en kA.
Je lui ai fait un écran personnalisé en A qui lui convient.
Il faudrait avoir la possibilité de changer les unités sur les écrans de base, ce n'est pas la première fois que l'on a des retours client à ce sujet.
Cdlt
You’ve reached the end of your document
Create your free account or log in to subscribe to the board - and gain access to more than 10,000+ support articles along with insights from experts and peers.