Our Community ranking system has recently been updated. You may notice changes in user rankings and receive system messages or notifications. If you have questions about how the new ranking works, please refer to the announcement post for more details (click here).

PM8000 Alarming & Data Export

Metering & Power Quality

Schneider Electric support forum about Power Meters (ION, PowerTag, PowerLogic) and Power Quality from design, implementation to troubleshooting and more.
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
  • PM8000 Alarming & Data Export
Options
  • Mark Topic as New
  • Mark Topic as Read
  • Float this Topic for Current User
  • Bookmark
  • Subscribe
  • Mute
  • Printer Friendly Page
Invite a Co-worker
Send a co-worker an invite to the portal.Just enter their email address and we'll connect them to register. After joining, they will belong to the same company.
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
582
Mehran_Mehrnia
Mehran_Mehrnia Champion
216
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
SekherNK
SekherNK Explorer
Explorer

Posted: ‎2022-02-08 06:54 PM

1 Like
3
3476
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
‎2022-02-08 06:54 PM

PM8000 Alarming & Data Export

Hi,

 

I have a few questions regarding exporting of alarms and datalogs from PM8240.

 

In a site without PME, can PM8000 send alarms and data logs to a 3rd party system (for eg: BMS or SCADA)?

What is the format of the datalog native export?

What are the comms protocol that PM8000 supports to export the data to such 3rd party systems(e.g FTP, Modbus etc)?

 

Thanks,

Sekher

 

Labels
  • Labels:
  • PM8000
Tags (1)
  • Tags:
  • english
Reply
  • All forum topics
  • Previous Topic
  • Next Topic

Accepted Solutions
Charles_Murison
Charles_Murison Champion
Champion

Posted: ‎2022-02-09 04:41 PM

2 Likes
2
3459
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
‎2022-02-09 04:41 PM

Hello @SekherNK ,

 

Regarding datalogs there are only 2 ways to export from the meter. The first is to use propriety protocol called ION with software such as ION Setup, Power Monitoring Expert or Power Operation. 

 

The second option is with a module called Log Export module. Refer to ION Reference for more details. In Summary the meter will send email with log data attached as an xml file.

 

It may be possible to transfer Alarm state with modbus however alarm data that you would see from meter's front panel only supported with ION protocol.

 

Regards,

Charles

L4 Prime for Advanced metering and Utilities

See Answer In Context

Tags (1)
  • Tags:
  • english
Reply
Replies 3
Charles_Murison
Charles_Murison Champion
Champion

Posted: ‎2022-02-09 04:41 PM

2 Likes
2
3459
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
‎2022-02-09 04:41 PM

Hello @SekherNK ,

 

Regarding datalogs there are only 2 ways to export from the meter. The first is to use propriety protocol called ION with software such as ION Setup, Power Monitoring Expert or Power Operation. 

 

The second option is with a module called Log Export module. Refer to ION Reference for more details. In Summary the meter will send email with log data attached as an xml file.

 

It may be possible to transfer Alarm state with modbus however alarm data that you would see from meter's front panel only supported with ION protocol.

 

Regards,

Charles

L4 Prime for Advanced metering and Utilities
Tags (1)
  • Tags:
  • english
Reply
Anonymous user
Not applicable

Posted: ‎2022-10-10 11:27 PM

0 Likes
1
3336
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
‎2022-10-10 11:27 PM

Hi Charles,

 

Following on from this I have a PM8000 setup and have configured it to send emails to a local SMTP server (in this case I have setup Mailslurper on a local machine in same subnet as meter) when frequency events are recorded.

 

The emails are getting sent however the emails being received by Mailslurper do not have an XML file attached. They instead have mainly timestamps in them as per the screenshot. The data recorders setup to be captured have Freq, Voltage and kW from Power Meter module. If I do a manual Data Recorders Collect through Ion Setup Assistant I can see that data recorder is capturing data correctly in the xml file.

 

This may be an issue with how Mailslurper decodes the emails but was wondering if there is anything I should check on the PM8000 configuration side to make sure the data is attached as an XML file? In particular potentially in the Log Export modle under 'Setup Registers' there is a field 'Attachment Extention' which defaults to MMA.

 

Finally when configuring an smtp email send on a PM8000 can credentials be added so that a secure email is sent?

Attachments
Tags (1)
  • Tags:
  • english
Reply
Charles_Murison
Charles_Murison Champion
Champion

Posted: ‎2022-10-11 02:00 PM

0 Likes
0
3328
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
‎2022-10-11 02:00 PM

Hello @Anonymous user 

 

"when configuring an smtp email send on a PM8000 can credentials be added so that a secure email is sent?" No only simple SMTP is supported at this time.

 

"anything I should check on the PM8000 configuration side to make sure the data is attached as an XML file?" Should not have to. Note that file extension may be .mma, however the contents of the file will be xml. I have never used that mail program so I do not know what is done with attachments.

 

I have done packet capture files in the past so I know the data is sent from meter to SMTP server as an attached file. 

 

Regards

Charles

L4 Prime for Advanced metering and Utilities
Tags (1)
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
Create your free account or log in to subscribe to the board - and gain access to more than 10,000+ support articles along with insights from experts and peers.