Ask our Experts
Didn't find what you are looking for? Ask our experts!
New Community Ranking System
Our Community ranking system has recently been updated. You may notice changes in user rankings and receive system messages or notifications. If you have questions about how the new ranking works, please refer to the announcement post for more details (click here).
Schneider Electric support forum about Power Meters (ION, PowerTag, PowerLogic) and Power Quality from design, implementation to troubleshooting and more.
Search in
Please select a country to continue with beta search.
Link copied. Please paste this link to share this article on your social media post.
Hi all,
Need your help please. This is what my customer has asked.
Can you please confirm.
Just a query; do you know the max devices that the PAS800 can handle officially also what is the “recommended” limit?
As in I know Com’X510 could connect up to 64 meters but it started to struggle with a lot less than that.
I am looking at a project where they want to connect 78 PM5560 meters to a ComX510. Would the PAS800 be suitable for this application or no?
Link copied. Please paste this link to share this article on your social media post.
Hello @JohnBoskovski ,
Better ask on the dedicated channel:
https://community.se.com/t5/Gateways-and-Energy-Servers/bd-p/gateways-energy-servers
Please also have a look on the Panel Server Catalog to learn more about some limitations:
Panel Server Advanced and Universal are supporting max 64 downstream TCP connections (ETH devices). You can also connect up to 32 Serial devices without repeater. But just like Com'X, you may face some performance issues if you connect to much devices. For the moment, we have no documentation giving a "weight" per device and mentioning what is the maximum "weight" for the Panel Server.
Now my questions:
In any case, the Panel Server may not be suitable for all 78 PM5560. You may need to divide your architecture with 2x PAS800 with 39x PM5000 connected to each.
Regards,
Link copied. Please paste this link to share this article on your social media post.
Hello @JohnBoskovski ,
Better ask on the dedicated channel:
https://community.se.com/t5/Gateways-and-Energy-Servers/bd-p/gateways-energy-servers
Please also have a look on the Panel Server Catalog to learn more about some limitations:
Panel Server Advanced and Universal are supporting max 64 downstream TCP connections (ETH devices). You can also connect up to 32 Serial devices without repeater. But just like Com'X, you may face some performance issues if you connect to much devices. For the moment, we have no documentation giving a "weight" per device and mentioning what is the maximum "weight" for the Panel Server.
Now my questions:
In any case, the Panel Server may not be suitable for all 78 PM5560. You may need to divide your architecture with 2x PAS800 with 39x PM5000 connected to each.
Regards,
You’ve reached the end of your document
Create your free account or log in to subscribe to the board - and gain access to more than 10,000+ support articles along with insights from experts and peers.