Ask our Experts
Didn't find what you are looking for? Ask our experts!
New Community Ranking System
Our Community ranking system has recently been updated. You may notice changes in user rankings and receive system messages or notifications. If you have questions about how the new ranking works, please refer to the announcement post for more details (click here).
Schneider Electric support forum about Power Meters (ION, PowerTag, PowerLogic) and Power Quality from design, implementation to troubleshooting and more.
Search in
Please select a country to continue with beta search.
Posted: 2020-02-10 10:08 PM
Link copied. Please paste this link to share this article on your social media post.
Link copied. Please paste this link to share this article on your social media post.
Hello @Anonymous user
The latest firmware version for PM3255 is v1.5.01 which enabled the field firmware upgrade support. There no new firmware released after v1.5.01 to upgrade in the field.
Regards,
Ramasamy N
Link copied. Please paste this link to share this article on your social media post.
Hey @Anonymous user , thank you for your question
I moved it to the Power Metering forum where the community of experts will be able to provide you the right support and solve your issue!
PS: don't hesitate to check the Knowledge base and use the search bar with keywords. there is a lot of content discussed everyday and your issue may have already been solved 😉
Posted: 2020-02-17 06:46 AM
Link copied. Please paste this link to share this article on your social media post.
Thanks Omaelk
I still couldn't find any firmware downloads for the PM3255 meters. I have searched the Knowledge base the web so I would appreciate if someone can assist me regarding this.
Regards
Marius
Link copied. Please paste this link to share this article on your social media post.
Hello @Anonymous user ,
Would you be able to answer this question?
Charles
Link copied. Please paste this link to share this article on your social media post.
Posted: 2020-05-25 02:52 AM
Link copied. Please paste this link to share this article on your social media post.
Thanks Ramasemy
My meters still have V1.0.09 on it so I would love to upgrade it to V1,5.01. Where can I download the Firmware?
Regards
Marius
Link copied. Please paste this link to share this article on your social media post.
Hello Marius,
The PM3255 firmware version v1.0.09 does not support to upgrade the the firmware v1.5.01 in the field.
Only the new meters are produced with the firmware v1.5.01, so they can buy new meter if they really want PM3255 with latest firmware.
Regards,
Ramasamy N
Posted: 2021-12-23 07:27 AM
Link copied. Please paste this link to share this article on your social media post.
Afternoon All,
I too would like to have the firmware to upgrade a couple of meters I have that seems to be bit buggy. One of them is on V1.3 and I am struggling to get the connection and interface to a 3rd party modem sorted even though the port and other communication settings are correct If I use those exact settings via a ComX device I can connect the meter. but then I have to have a gateway behind another gateway
I have exactly the same setup on the other side of the building and that seems to be functional where I have a direct connection between the meter and the modem. I have duplicated the same modem config to multiple other modems of the same firmware version and it doesn't work. If I take that same functional modem and connect it to the meter that I am struggling with it too doesn't connect, however if I test the comport directly it works on that meter., so it is definitely a meter issue.
Thank you in advance for your assistance
Christopher
You’ve reached the end of your document
Create your free account or log in to subscribe to the board - and gain access to more than 10,000+ support articles along with insights from experts and peers.