Our Community ranking system has recently been updated. You may notice changes in user rankings and receive system messages or notifications. If you have questions about how the new ranking works, please refer to the announcement post for more details (click here).

No password for a PM5561?

Metering & Power Quality

Schneider Electric support forum about Power Meters (ION, PowerTag, PowerLogic) and Power Quality from design, implementation to troubleshooting and more.
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
  • No password for a PM5561?
Options
  • Mark Topic as New
  • Mark Topic as Read
  • Float this Topic for Current User
  • Bookmark
  • Subscribe
  • Mute
  • Printer Friendly Page
Invite a Co-worker
Send a co-worker an invite to the portal.Just enter their email address and we'll connect them to register. After joining, they will belong to the same company.
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
581
Mehran_Mehrnia
Mehran_Mehrnia Champion
216
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
Philippe_Morel
Philippe_Morel Mentor
Mentor

Posted: ‎2016-10-24 06:15 AM . Last Modified: ‎2020-04-22 01:22 AM

0 Likes
1
1143
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
‎2016-10-24 06:15 AM

No password for a PM5561?

A client asks me why he does not have to use a password when making changes to the alarmes of a PM5561 with ION Setup?

 

BR,

Philippe

Labels
  • Labels:
  • ION Setup
Reply
  • All forum topics
  • Previous Topic
  • Next Topic

Accepted Solutions
Robert_Lee
Robert_Lee Champion
Champion

Posted: ‎2016-10-28 09:11 AM

0 Likes
0
1112
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
‎2016-10-28 09:11 AM

Most of the PM5000 series of the device do not extend their password security to communications (unlike most of our more advanced ION products).  There are a few protected functions (like upgrading a PM5000 which requires the top level user logon/password) but otherwise the only requirement is that the software is able to grab the semaphore (which essentially is a token to prevent multiple clients from making modifications at the same time which includes the front panel) when issuing any of the protect commands which allow users to configure/control the device remotely.

Adding security to the actual device would require firmware changes and then subsequent ION Setup changes as well to support that change.

See Answer In Context

Reply
Reply 1
Robert_Lee
Robert_Lee Champion
Champion

Posted: ‎2016-10-28 09:11 AM

0 Likes
0
1112
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
‎2016-10-28 09:11 AM

Most of the PM5000 series of the device do not extend their password security to communications (unlike most of our more advanced ION products).  There are a few protected functions (like upgrading a PM5000 which requires the top level user logon/password) but otherwise the only requirement is that the software is able to grab the semaphore (which essentially is a token to prevent multiple clients from making modifications at the same time which includes the front panel) when issuing any of the protect commands which allow users to configure/control the device remotely.

Adding security to the actual device would require firmware changes and then subsequent ION Setup changes as well to support that change.
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
Create your free account or log in to subscribe to the board - and gain access to more than 10,000+ support articles along with insights from experts and peers.