Ask our Experts
Didn't find what you are looking for? Ask our experts!
New Community Ranking System
Our Community ranking system has recently been updated. You may notice changes in user rankings and receive system messages or notifications. If you have questions about how the new ranking works, please refer to the announcement post for more details (click here).
Schneider Electric support forum about Power Meters (ION, PowerTag, PowerLogic) and Power Quality from design, implementation to troubleshooting and more.
Search in
Please select a country to continue with beta search.
Link copied. Please paste this link to share this article on your social media post.
Post a list of devices you'd want to see support added (either as a native device or just a Modbus folder).
Here's a list of native devices presently supported by ION Setup today:
| Schneider Electric | SquareD | Siemens | Power Measurement Ltd. | Other |
|---|---|---|---|---|
|
ION8800 Power Meter ION7400 Power Meter ION7550 Power Meter ION7650 Power Meter ION8650 Power Meter PowerLogic BCPM PowerLogic BCPME EasyLogic DM6200 Digital Meter EasyLogic DM6300 Digital Meter PowerLogic E5600 Energy Meter EasyLogic EM1200 Energy Meter EasyLogic EM1220 Energy Meter EasyLogic EM1350 Energy Meter PowerLogic EM3550 Energy Meter PowerLogic EM3555 Energy Meter PowerLogic EM4235 Enercept PowerLogic EM4236 Enercept PowerLogic EM4900 MCM2 PowerLogic EM6400 Energy Meter PowerLogic EM6400NG Energy Meter PowerLogic EM6430 Energy Meter PowerLogic EM6433 Energy Meter PowerLogic EM6434 Energy Meter PowerLogic EM6435 Energy Meter PowerLogic EM6436 Energy Meter PowerLogic EM6438 Energy Meter PowerLogic EM6459 Energy Meter PowerLogic EM7230 Energy Meter PowerLogic EM7280 Energy Meter PowerLogic EM7290 Energy Meter PowerLogic Enercept Meter PowerLogic Enercept E23C6 Meter PowerLogic iEM3150 Energy Meter PowerLogic iEM3155 Energy Meter PowerLogic iEM3250 Energy Meter PowerLogic iEM3255 Energy Meter PowerLogic iEM3350 Energy Meter PowerLogic iEM3355 Energy Meter PowerLogic iEM3455 Energy Meter PowerLogic iEM3555 Energy Meter EasyLogic PM1200 Power Meter EasyLogic PM2120 Power Meter EasyLogic PM2125 Power Meter EasyLogic PM2130 Power Meter EasyLogic PM2220 Power Meter EasyLogic PM2225 Power Meter EasyLogic PM2230 Power Meter PowerLogic PM3250 Power Meter PowerLogic PM3255 Power Meter PowerLogic PM5110 Power Meter PowerLogic PM5111 Power Meter PowerLogic PM5310 Power Meter PowerLogic PM5311 Power Meter PowerLogic PM5320 Power Meter PowerLogic PM5330 Power Meter PowerLogic PM5331 Power Meter PowerLogic PM5340 Power Meter PowerLogic PM5341 Power Meter PowerLogic PM5350 Power Meter PowerLogic PM5560 Power Meter PowerLogic PM5561 Power Meter PowerLogic PM5563 Power Meter PowerLogic PM8000 Power Meter ION9000 Power Meter |
PowerLogic PM200 Power Meter PowerLogic PM600 Power Meter PowerLogic PM620 Power Meter PowerLogic PM650 Power Meter PowerLogic PM700 Power Meter PowerLogic PM750 Power Meter PowerLogic PM810 Power Meter PowerLogic PM820 Power Meter PowerLogic PM850 Power Meter PowerLogic PM870 Power Meter PowerLogic CM2050 Circuit Monitor PowerLogic CM2150 Circuit Monitor PowerLogic CM2250 Circuit Monitor PowerLogic CM2350 Circuit Monitor PowerLogic CM2450 Circuit Monitor PowerLogic CM3250 Circuit Monitor PowerLogic CM3350 Circuit Monitor PowerLogic CM4000T Circuit Monitor PowerLogic CM4250 Circuit Monitor |
4300 Power Meter 4700 Power Meter 4720 Power Meter 9200 Power Meter 9300 Power Meter 9330 Power Meter 9340 Power Meter 9350 Power Meter 9360 Power Meter 9410 Power Meter 9500 Power Meter 9500 RTU 9510 Power Meter 9510 RTU 9600 Power Meter 9610 Power Meter 9700 Power Meter |
3300 ACM Power Meter 3350 PDM Power Demand Monitor 3710 ACM Power Meter 3720 ACM Power Meter 3750 PDC Demand Controller 3800 RTU ION6200 Power Meter ION6300 Power Meter ION7300 Power Meter ION7330 Power Meter ION7350 Power Meter ION7500 Power Meter ION7500 RTU ION7550 Power Meter ION7550 RTU ION7600 Power Meter ION7650 Power Meter ION7700 Power Meter ION8300 Power Meter ION8400 Power Meter ION8500 Power Meter ION8600 Power Meter ION8800 Power Meter |
Allen-Bradley 1400 PB Power Meter Allen-Bradley 1400 PD Power Meter ABB 8300 Power Meter ABB 8400 Power Meter ABB 8500 Power Meter GE 7700 ION Power Meter |
List of supported Modbus RTU-based devices:
Link copied. Please paste this link to share this article on your social media post.
Thanks Rob,
We would like to put our vote in for the following devices:
EM4800
MicroLogic Trip Units
NSX Breakers
If you need any further clarification, let me know.
Link copied. Please paste this link to share this article on your social media post.
I'm looking into at least add some type of support for the Micrologic Trip Units already (PowerPact Models A/P/H and something for the Masterpact) but am unfamiliar with the EM4800 and NSX Breakers.
Would you happen to have some documentation on the Modbus maps for those devices?
Would also help if I could get remote access to some of these as well.
Link copied. Please paste this link to share this article on your social media post.
Hi Robert,
EM4800 is a third party device supplied by Triacta and is equivalent of Triacta Power Hawk range. It would be great if we could have EM4800 configuration as well in ION Setup. Currently we use SE Metershop or a Schneider-ised version of Triacta tool and it is not very user friendly.
Also Compact NSX Micrologic and Micrologics for Compact NS and Masterpact share a lot of common registers too.
I am including the modbus list for both for your reference.
Looking forward to see if its possible to include those in it.
Link copied. Please paste this link to share this article on your social media post.
Hi Hastak,
Thanks for the information and when I get a chance I'll take a look at the map and see how easy it is to implement and check around if we have a EM4800 somewhere at Betram that I can try to interface to.
Link copied. Please paste this link to share this article on your social media post.
Just out of curious, what kind action/info you would like to do to MLTU and NSX breakers in ION Setup?
I normally only need to set up all communication parameters right from the front panel and they are good to go in the monitoring perspective. For NSX, I believe the only thing required is the modbus address, and the IFM module will auto-adapt to the RS485 baud rate and parity.
Except that, all other parameters are related to the protection settings (maybe data and time are common settings), and should be set up by the breaker guys rather than monitoring guys like myself. As far as I know, there ARE software (like RSU, LSU...) from other entity of Schneider to set these parameter up.
Anyway, my points is ION setup should NOT have the capability to mess up any protection parameters, they should be left alone to the specified existing software. Under this assumption, wonder what else ION setup can do with these trip units? Maybe sync the time and view the real time data?
Link copied. Please paste this link to share this article on your social media post.
I would like to see support for PM6. I currently have a customer that has migrated from SMS to PME. The migration has not been pretty and this is another blemish to the issues they have been suffering. Currently our documentation still refers to SMS and we have to tell them to use PMCU. They are not happy at all.
Link copied. Please paste this link to share this article on your social media post.
The lastest progress on PM6 can be found here Re: Needs PM600 meter support in ION Setup. I believe I put in this request when I first came off site from the customer you mentioned, we are making some progress, as the newest ION setup can set up basic parameters and on-board logs in PM6, but not the on-board alarms yet.
Regards,
Link copied. Please paste this link to share this article on your social media post.
PM600 alarm support should now be available in 3.0.14077.03 available on Box/FTP.
Its still very preliminary and there could be some issues still as I try to find available time to do further testing. Any issue(s) found, please report them directly to me via e-mail.
Link copied. Please paste this link to share this article on your social media post.
Also looked into supporting the EM4800 and it doesn't look like it supports device configuration via Modbus (the Triacta software tools seems to use some type of Telnet interface). Without any further documentation, it would be ill advised and time consuming to attempt to replicate that functionality and unless we want to add just viewing support, then it might just not be worth looking into this further.
Link copied. Please paste this link to share this article on your social media post.
Hi Robert,
I created my first knowledgebase article on the topic of device support in ION Setup here.
I will try to update it periodically as you release newer versions of the software.
Link copied. Please paste this link to share this article on your social media post.
SIM 10 modules would be useful.
Link copied. Please paste this link to share this article on your social media post.
I've never heard of SIM 10 modules (who manufactures them). Do they communicate Modbus? One could manually add a generic Modbus driver to an existing deployment using just Notepad (clue: Open some of the files found in the TABLES\Modbus\... subfolders using Notepad and you can figure out stuff fairly easily at least to view real-time info). But any added devices to the device list would need to have a sufficient use case to have me add primary support in the software.
Link copied. Please paste this link to share this article on your social media post.
Link copied. Please paste this link to share this article on your social media post.
Maybe a long shot but what about the PM9c (old PM meter) ?
We have sold many of these untill they became obsolete.
Link copied. Please paste this link to share this article on your social media post.
By the looks of the PDF you attached, these old circuit breakers only communicated using Sy/Max protocol (original SquareD protocol) which ION Setup presently doesn't communicate natively. If one of the gateway products like EGX or ComX has a Modbus TCP translator (like it does for the CM2xxx), then it might be feasible to add some of the registers in ION Setup for viewing (and/or you could set something up in PME using the MDI).
Being a protection device, I would hesitate in attempting to implement any type of configuration support in ION Setup due to the nature of the product (and likely complexity).
Link copied. Please paste this link to share this article on your social media post.
Robert:
Once the meter goes though a gateway this is translated to Modbus.
Thanks,
Michael
Posted: 2017-04-07 04:58 AM
Link copied. Please paste this link to share this article on your social media post.
Hi ,
I have issue with configuration of the ION enterprise version 7.2.1 with new device of PM2120. there is a error message as " valid version "
I used following link for configuration
http://www.schneider-electric.co.in/en/download/document/PM2000_Series_SE_Driver_PME_7.2.2_ENG/
Please kindly informed me where i can find the ION enterprise version 7.2.1 driver to setup the above meter..
Best Regards,
Sandamali Gunathilaka
Link copied. Please paste this link to share this article on your social media post.
Hello Sandamali,
1) ION Setup and PME are 2 separate sofware
2) The driver name indicates that this supports PME 7.2 SP2, you will need to upgrade PME to 7.2.2 to use the driver. It is very likely there is no driver for PME 7.2.1
Link copied. Please paste this link to share this article on your social media post.
Vote for all the Square D PowerLogic meters since there are so many in the field now.
You’ve reached the end of your document
Create your free account or log in to subscribe to the board - and gain access to more than 10,000+ support articles along with insights from experts and peers.