Send a co-worker an invite to the Exchange portal.Just enter their email address and we’ll connect them to register. After joining, they will belong to the same company.
Send Invite Cancel
84792members
354240posts

Need IEEE519-2014 framework and diagram for upload to ION7650

Metering & Power Quality

Collaborate with multiple experts and discuss various topics about Power Meters and Power Quality. From design & implementation to troubleshooting and more, get support from experts and share your experiences by subscribing to the Schneider Electric Exchange forum today.

Solved
sesa101781_brid
Ensign Ensign
Ensign
0 Likes
5
1458

Need IEEE519-2014 framework and diagram for upload to ION7650

Hi, I need IEEE519-2014 framework and diagram for upload to ION7650.

 

I have seen in PME9.0 demo website that ION9k has IEEE519 icon at the diagram (see attached). This icon will show 95% percentile & 99% percentile of harmonic measurement (see attached) but I can’t see what is the details inside that icon and what is the framework of IEEE519.

 

I try to paste from ION9k framework provided by PME9.0 in designer by myself but all links are broken (see attached).

 

Therefore, I need diagram file and framework file from ION9k, those have complete link to all registers, to modify by myself. 

 

Hope someone can help me on this.

 

 

Attachments

Accepted Solutions
Tom_Stevenson
Picard Picard
Picard
0 Likes
0
1419

Re: Need IEEE519-2014 framework and diagram for upload to ION7650

Hi Chonnapan

 

The IEEE519-2014 framework and corresponding report in PME 9.0 is not available on the 7x50 platform.  It requires ION modules only available on the ION9000 and forthcoming PM8000 and ION7400 V2.0 releases.

 

Best regards


Tom

See Answer In Context

5 Replies 5
sesa101781_brid
Ensign Ensign
Ensign
0 Likes
4
1450

Re: Need IEEE519-2014 framework and diagram for upload to ION7650

To update about this issue, I can paste almost all modules of IEEE519 framework from ION9000 into the ION meters now. All links can be linked to all available modules those were pasted. But, after investigation, I think the paste is not successful because some ION modules don’t exist in the current firmware of the meters. Therefore, impossible to paste IEEE519 to them. I may need to wait for new firmware upgrade.

 

My next question is, when we can get new firmware update for ION7x50? I searched in Exchange and found that PM8k and ION7400 firmware V.2 will be released in Dec'18 or Jan'19. Can anyone inform me please?

 

Thank you in advance.

Chonnapan

ChenLiang
Schneider Alumni (Retired)
Schneider Alumni (Retired)
0 Likes
3
1444

Re: Need IEEE519-2014 framework and diagram for upload to ION7650

Hi Chonnapan,

 

I have a bfo case logged for you, will reply you through bfo soon.

sesa101781_brid
Ensign Ensign
Ensign
0 Likes
2
1440

Re: Need IEEE519-2014 framework and diagram for upload to ION7650

Thank you very much. bFO of this case is shown in link below.

 

https://se.my.salesforce.com/0061200000XMaECAA1/d?retURL=https%3A%2F%2Fse--c.na72.visual.force.com%2...

 

Do I need to do support request? Please advise.

ChenLiang
Schneider Alumni (Retired)
Schneider Alumni (Retired)
0 Likes
1
1434

Re: Need IEEE519-2014 framework and diagram for upload to ION7650

Hi Chonnapan,

There is one case open already:
https://se.my.salesforce.com/5001H00000qyZg9

I will reply to R Laxman Rao who is the L2 technical support in India.

Thanks
Leo

Tom_Stevenson
Picard Picard
Picard
0 Likes
0
1420

Re: Need IEEE519-2014 framework and diagram for upload to ION7650

Hi Chonnapan

 

The IEEE519-2014 framework and corresponding report in PME 9.0 is not available on the 7x50 platform.  It requires ION modules only available on the ION9000 and forthcoming PM8000 and ION7400 V2.0 releases.

 

Best regards


Tom