Our Community ranking system has recently been updated. You may notice changes in user rankings and receive system messages or notifications. If you have questions about how the new ranking works, please refer to the announcement post for more details (click here).

NTP Server For ION8650C Time Synchronization

Metering & Power Quality

Schneider Electric support forum about Power Meters (ION, PowerTag, PowerLogic) and Power Quality from design, implementation to troubleshooting and more.
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
  • NTP Server For ION8650C Time Synchronization
Options
  • Mark Topic as New
  • Mark Topic as Read
  • Float this Topic for Current User
  • Bookmark
  • Subscribe
  • Mute
  • Printer Friendly Page
Invite a Co-worker
Send a co-worker an invite to the portal.Just enter their email address and we'll connect them to register. After joining, they will belong to the same company.
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
582
Mehran_Mehrnia
Mehran_Mehrnia Champion
216
Ramasamy_N
Ramasamy_N Champion
117
View All

Recommended Forums

  • SmartConnector Forum

Related Products
product field
PowerLogic
PowerLogic ION8650 series
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
Mariana17
Mariana17
Explorer

Posted: ‎2023-08-02 07:26 AM

1 Like
1
2414
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
‎2023-08-02 07:26 AM

NTP Server For ION8650C Time Synchronization

Hello community!

 

I have an GPS, model GE Reason RT3000-R2, which has the feature of NTP server. I would like to sync the ION8650C time with it. So, I set up the power meter as follows:

 

In the Clock menu:

Mariana17_0-1690983818025.png

In Communication > Advanced Ethernet > NTP:

Mariana17_0-1690985673225.png

 

At first the meter did not receive any response from the GPS, the synchronization failed. Because there was no communication between meter and GPS.

Mariana17_1-1690986227901.png

After making a network change, the meter synchronized with a totally wrong time. At one point, I figured the time on the GPS was wrong.

Mariana17_2-1690986250945.png

But the value of “Time Sync Count” did not increase at any time. That is, the time has changed, but it is as if the meter has not received an update request from the server through this protocol.

At one point the meter was set to “Line Freq”, it may have been synchronized in some other way? Or even be syncing with the NTP server without incrementing this value? Currently, it is varying between two dates, would it be syncing internally with the crystal and then with the GPS, alternately, without changing the value of “Time Sync Count”? 

 

 

  • Thumbnail of PowerLogic ION8650 series
    PowerLogic
    PowerLogic ION8650 series
View products (1)
Labels
  • Labels:
  • ION Setup
Tags (1)
  • Tags:
  • english
Reply
  • All forum topics
  • Previous Topic
  • Next Topic

Accepted Solutions
Charles_Murison
Charles_Murison Champion
Champion

Posted: ‎2023-08-02 08:54 AM

2 Likes
0
2406
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
‎2023-08-02 08:54 AM

Hello @Mariana17 ,

 

A few items to discuss on your post

1) "Value of “Time Sync Count” did not increase at any time. " When meter is set to NTP sadly this register does not update. The event log messages "Time about to change" and "Time Change" shows that meter is time sync'd with NTP server.

 

2) The different time ranges would suggest that something in the NTP message to the meter is not what the meter expects. The NTP time packet has 4 elements used by the meter, Reference Timestamp, Originate Timestamp, Receive Timestamp, Transmit Timestamp. The meter will do some math with these timestamps and use the results to calculate what change needs to happen. 

What I have seen happen in the past is inside the NTP packet from NTP source, the time for Transmit Timestamp is less than Receive Timestamp. Physical this cannot happen as the NTP source cannot send out a message before it has received the message asking for NTP response be sent. The math inside the meter will create a large negative number that the meter then applies to the current timestamp resulting in the shift to 2091.

Would need to confirm this is happening with a packet capture like Wireshark. Not always easy to capture the traffic, usually need a switch where port forwarding can mirror all network traffic to/from meter.

 

Regards,

Charles

L4 Prime for Advanced metering and Utilities

See Answer In Context

Reply
Reply 1
Charles_Murison
Charles_Murison Champion
Champion

Posted: ‎2023-08-02 08:54 AM

2 Likes
0
2406
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
‎2023-08-02 08:54 AM

Hello @Mariana17 ,

 

A few items to discuss on your post

1) "Value of “Time Sync Count” did not increase at any time. " When meter is set to NTP sadly this register does not update. The event log messages "Time about to change" and "Time Change" shows that meter is time sync'd with NTP server.

 

2) The different time ranges would suggest that something in the NTP message to the meter is not what the meter expects. The NTP time packet has 4 elements used by the meter, Reference Timestamp, Originate Timestamp, Receive Timestamp, Transmit Timestamp. The meter will do some math with these timestamps and use the results to calculate what change needs to happen. 

What I have seen happen in the past is inside the NTP packet from NTP source, the time for Transmit Timestamp is less than Receive Timestamp. Physical this cannot happen as the NTP source cannot send out a message before it has received the message asking for NTP response be sent. The math inside the meter will create a large negative number that the meter then applies to the current timestamp resulting in the shift to 2091.

Would need to confirm this is happening with a packet capture like Wireshark. Not always easy to capture the traffic, usually need a switch where port forwarding can mirror all network traffic to/from meter.

 

Regards,

Charles

L4 Prime for Advanced metering and Utilities
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
Create your free account or log in to subscribe to the board - and gain access to more than 10,000+ support articles along with insights from experts and peers.