Our Community ranking system has recently been updated. You may notice changes in user rankings and receive system messages or notifications. If you have questions about how the new ranking works, please refer to the announcement post for more details (click here).

Metering and Monitoring systems

Metering & Power Quality

Schneider Electric support forum about Power Meters (ION, PowerTag, PowerLogic) and Power Quality from design, implementation to troubleshooting and more.
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
  • Metering and Monitoring systems
Options
  • Mark Topic as New
  • Mark Topic as Read
  • Float this Topic for Current User
  • Bookmark
  • Subscribe
  • Mute
  • Printer Friendly Page
Invite a Co-worker
Send a co-worker an invite to the portal.Just enter their email address and we'll connect them to register. After joining, they will belong to the same company.
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
582
Mehran_Mehrnia
Mehran_Mehrnia Champion
217
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
Johan_2023
Johan_2023
Explorer

Posted: ‎2023-11-27 10:13 AM

0 Likes
2
1738
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
‎2023-11-27 10:13 AM

Metering and Monitoring systems

Hi there,
I recently did a Schneider online course "Metering and monitoring systems for power reliability and availability".  In this course, some core features were mentioned for the meters, and I have a question about one of these features.

Power Meters (Incoming) : Individual Harmonics up to 511th 

Power Meters (Critical Loads) : Individual Harmonics up to 127th 

Power Meters (Feeder) : Individual Harmonics up to 31th 

I would like to know the technical reason for these 511, 127 and 31 th. Is there any technical reason why the incoming need to measure up to 511 th (and not up to 127 instead)? and same for Critical loads 127th and feeder 31?

What happens if the incoming can't detect up to 511?

 

My question is because when I specify these features in the EMS technical specification, normally the client ask me "Why 511th, why 127 and why 31". 

 

Why not only 127 for the incoming if after the 100th the effects are not considerable?


Thanks



Attachments
Labels
  • Labels:
  • Power Quality
Tags (1)
  • Tags:
  • english
Reply
  • All forum topics
  • Previous Topic
  • Next Topic

Accepted Solutions
DanL
DanL Champion
Champion

Posted: ‎2023-11-30 03:42 PM

1 Like
0
1717
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
‎2023-11-30 03:42 PM

technically, meters will often have other limits besides just the Nyquist limitation for harmonic bandwidth.

https://en.wikipedia.org/wiki/Nyquist_frequency

 

For example if the device implements a low-pass filter (such as required by IEC 61000-4-30 Class A) then on some designs, although it may be mathematically capable of registering a result for the "255th harmonic" from a captured waveform, the reading may not be valid or useful (b/c the signal was attenuated below the noise floor)

See Answer In Context

Reply
Replies 2
Charles_Murison
Charles_Murison Champion
Champion

Posted: ‎2023-11-29 09:16 AM

0 Likes
1
1732
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
‎2023-11-29 09:16 AM

Hello @Johan_2023 ,

 

The maximum harmonic for a meter to be able to detect is (n/2 -1) where n is the sample rate. So a meter with sample rate of 1024 samples per cycle can have a maximum of 511th harmonic. 

 

Regards,

Charles

L4 Prime for Advanced metering and Utilities
Reply
DanL
DanL Champion
Champion

Posted: ‎2023-11-30 03:42 PM

1 Like
0
1717
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
‎2023-11-30 03:42 PM

technically, meters will often have other limits besides just the Nyquist limitation for harmonic bandwidth.

https://en.wikipedia.org/wiki/Nyquist_frequency

 

For example if the device implements a low-pass filter (such as required by IEC 61000-4-30 Class A) then on some designs, although it may be mathematically capable of registering a result for the "255th harmonic" from a captured waveform, the reading may not be valid or useful (b/c the signal was attenuated below the noise floor)
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
Create your free account or log in to subscribe to the board - and gain access to more than 10,000+ support articles along with insights from experts and peers.