Send a co-worker an invite to the Exchange portal.Just enter their email address and we’ll connect them to register. After joining, they will belong to the same company.
Send Invite Cancel
84351members
353531posts

ION9000 (HEP) - ION modules increase

Metering & Power Quality

Collaborate with multiple experts and discuss various topics about Power Meters and Power Quality. From design & implementation to troubleshooting and more, get support from experts and share your experiences by subscribing to the Schneider Electric Exchange forum today.

Solved
Daniel_Brandao
Lt. Commander Lt. Commander
Lt. Commander

ION9000 (HEP) - ION modules increase

Hi everyone, with ION9000 release we increased the number of several ION modules, please see below for details. Also, now arythmetic modules can have up to 16 inputs.

 

There will also be increases on PM8000 / 7400 modules in the next firmware release (V2.0). The next PM8000 / ION7400 firmware will be available late December / early January.

 

 ION modules.jpg

Attachments

Accepted Solutions
Daniel_Brandao
Lt. Commander Lt. Commander
Lt. Commander
0 Likes
0
717

Re: ION9000 (HEP) - ION modules increase

No plans for ION module and PQ updates on 7X50 platform. The changes planned in this platform are all related to cybersecurity.

See Answer In Context

5 Replies 5
sesa101781_brid
Ensign Ensign
Ensign
0 Likes
2
749

Re: ION9000 (HEP) - ION modules increase

Hello,

 

As your said, new firmware V.2 for PM8k and ION7400 will be released with new ION module. How about ION7x50? Are there any news for new firmware upgrade? I need to upload IEEE519 framework to ION7650 that may require new modules (should be "Sort" modules). Please advise.

 

Thank you in advance.

Chonnapan

ChenLiang
Schneider Alumni (Retired)
Schneider Alumni (Retired)
0 Likes
0
742

Re: ION9000 (HEP) - ION modules increase

Hi Chonnapan,

 

I have a bfo case logged for you, will reply you through bfo soon.

Charles_Murison
Picard Picard
Picard
0 Likes
1
734

Re: ION9000 (HEP) - ION modules increase

With the increase to the number of inputs allowed to arithmatic modules, will there be any changes to the default templates to make use of this feature?

L4 Prime for Advanced metering and Utilities
Cliff_Schubert
Lieutenant JG Lieutenant JG
Lieutenant JG

Re: ION9000 (HEP) - ION modules increase

There have been some updates and optimization in the PQ section of the framework.

Daniel_Brandao
Lt. Commander Lt. Commander
Lt. Commander
0 Likes
0
718

Re: ION9000 (HEP) - ION modules increase

No plans for ION module and PQ updates on 7X50 platform. The changes planned in this platform are all related to cybersecurity.