Posted: 2019-09-19 10:31 AM
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
Hi Grant, Rich,
The low voltage DC variant of the ION9000 meter is in the plan, but I don't have details on the current roadmap, I believe James @Fabian_Decobecq would be able to give further details.
Regarding the PM8000, the low voltage DC version (24V) is already available as an active commercial reference.
Regards,
Fabricio

Posted: 2019-08-02 08:07 AM
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
Hi @Grant_IPACS ,
I have noticed that your topic is still unanswered.
I was wondering if you found a solution on your side. If you did, I kindly invite you to share it with the community. 🙂
If you still haven't found a solution, please do not hesitate to inform us.
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
Hi @Anonymous user no official answer as yet.
had to use UPS AC aux supply rather than battery backed DC supply to overcome the issue.
so many 7650's with ELV DC aux that we cannot recommend for upgrade just yet based on this.
Grant

Posted: 2019-09-13 12:51 AM
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
We are in the same situation, lots of 24VDC ION7650's out there that we can't replace, also people asking for 24VDC ION9000's in new installs
Can anybody at Schneider give us an update when we can expect at 24VDC variant ?
I also seem to remember from the PM8000 launch that was going to get 24VDC too but haven't seen that yet either
Cheers

Posted: 2019-09-13 02:08 AM . Last Modified: 2019-09-13 02:09 AM
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
Hi,
Thanks for your feedbacks both of you @Grant_IPACS and @Anonymous user
@Charles_Murison , do you think you can you help us on this topic please?
Thank you very much.

Posted: 2019-09-19 10:31 AM
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
Hi Grant, Rich,
The low voltage DC variant of the ION9000 meter is in the plan, but I don't have details on the current roadmap, I believe James @Fabian_Decobecq would be able to give further details.
Regarding the PM8000, the low voltage DC version (24V) is already available as an active commercial reference.
Regards,
Fabricio