Our Community ranking system has recently been updated. You may notice changes in user rankings and receive system messages or notifications. If you have questions about how the new ranking works, please refer to the announcement post for more details (click here).

ION8650 DNP Data Quality / Alarming

Metering & Power Quality

Schneider Electric support forum about Power Meters (ION, PowerTag, PowerLogic) and Power Quality from design, implementation to troubleshooting and more.
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
  • ION8650 DNP Data Quality / Alarming
Options
  • Mark Topic as New
  • Mark Topic as Read
  • Float this Topic for Current User
  • Bookmark
  • Subscribe
  • Mute
  • Printer Friendly Page
Invite a Co-worker
Send a co-worker an invite to the portal.Just enter their email address and we'll connect them to register. After joining, they will belong to the same company.
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
582
Mehran_Mehrnia
Mehran_Mehrnia Champion
216
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
sesa331493_brid
sesa331493_brid Leader
Leader

Posted: ‎2015-05-04 10:01 AM

0 Likes
1
1338
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
‎2015-05-04 10:01 AM

ION8650 DNP Data Quality / Alarming

I am trying to fulfill a requirement to get our ION 8650 Meter certified to use as a RIG on the CAISO control grid. I am running into a stumbling block on determining if our meter has sufficient DNP Quality and alarming.  Here is the requirement.

The RIG/DPG shall be able to send CAISO a data quality indication. The RIG/DPG shall provide a DNP ONLINE / OFFLINE quality flag on a per point basis. CAISO will fail and re-establish the communication to the external device.

The use of DNP ONLINE / OFFLINE quality flag is required for all analog points. When communication is lost with any external device the analog data associated with that device should indicate an OFFLINE status. The use of the DNP ONLINE / OFFLINE quality flag shall be set from within the RIG/DPG.

For example:

If there are two serial communication ports ‘A’ and ‘B’ connected to the RIG/DPG device and port ‘A’ fails, those points associated with port ‘A’ alone have their DNP data quality flags set to OFFLINE internally to the RIG/DPG. While port ‘B’ data points DNP remain set to ONLINE.

If external points are connected to a network LAN device and the LAN fails to communicate only those points associated to that LAN port have their DNP quality flags set to OFFLINE

I am not sure if the ION8650’s DNP modules are already designed to do this or if it would require modification. Most of the data coming into the meter will be modbus data coming in on the Ethernet, the meter being a Modbus master to several slave devices. The data will then be exported out of the meter through DNP. If one of the slave devices looses communication there needs to be a quality flag for that group of DNP values showing it as bad quality or Offline. The rest of the values need to stay online. 

Tags (3)
  • Tags:
  • dnp
  • dnp3
  • ion8650
Reply
  • All forum topics
  • Previous Topic
  • Next Topic
Reply 1
sesa44646
sesa44646 Leader
Leader

Posted: ‎2015-05-04 12:45 PM

0 Likes
0
1300
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
‎2015-05-04 12:45 PM

Hi Matthew - Moving this to Hardware community so it will get noticed.

- Vince
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
Create your free account or log in to subscribe to the board - and gain access to more than 10,000+ support articles along with insights from experts and peers.