ION7650 Which nominal voltage?

Metering & Power Quality

Schneider Electric support forum about Power Meters (ION, PowerTag, PowerLogic) and Power Quality from design, implementation to troubleshooting and more.
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
  • EcoStruxure Power & Grid
  • Metering & Power Quality
  • ION7650 Which nominal voltage?
Options
  • Mark Topic as New
  • Mark Topic as Read
  • Float this Topic for Current User
  • Bookmark
  • Subscribe
  • Mute
  • Printer Friendly Page
Invite a Co-worker
Send a co-worker an invite to the portal.Just enter their email address and we'll connect them to register. After joining, they will belong to the same company.
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
Charles_Murison
Picard Charles_Murison Picard
525
Mehran_Mehrnia
Admiral Mehran_Mehrnia Admiral
138
Ramasamy_N
Captain Ramasamy_N Captain
115
View All

Recommended Forums

  • SmartConnector Forum

Invite a Colleague

Found this content useful? Share it with a Colleague!

Invite a Colleague Invite
Solved Go to Solution
Back to Metering & Power Quality
Start a Topic
Solved
Philippe_Morel
Commander Philippe_Morel Commander
Commander

Posted: ‎2015-01-22 02:08 AM

0 Likes
3
1673
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
‎2015-01-22 02:08 AM

ION7650 Which nominal voltage?

Which nominal voltage should I use for this network (4W-WYE) so that the ION7650 takes waveforms? (15400.00V or 8891.19V ?)

(There is no real neutral conductor in the medium voltage station.)

5606

Is it enough to fill in the nominal voltage for getting waveforms, or do I still need to configure something else?

Tags (7)
  • Tags:
  • ion7650
  • mode
  • nominal
  • pme
  • voltage
  • volts
  • waveforms
Reply
  • All forum topics
  • Previous Topic
  • Next Topic

Accepted Solutions
Bojan
Admiral Bojan Admiral
Admiral

Posted: ‎2015-01-23 06:31 AM

0 Likes
0
1578
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
‎2015-01-23 06:31 AM

Hi Christine,

I think Philippe is asking about nominal voltage from Basic Setup, not Sag / Swell Module Settings - Nominal Voltage from Basic Setup is for harmonics calculation, and Nom Volts from Sag / Swell Module Settings is used for all Power Quality functions.

According to ION7650 / 7550 Programming Guide Nom Volts from Sag / Swell Module Settings is the primary power system voltage (sometimes different than PT Primary setup register value), which should be the same as Nominal Voltage from Basic Setup, I guess.

Best Regards,

Bojan

See Answer In Context

Reply
Replies 3
sesa70148
sesa70148 Schneider Alumni (Retired)
Schneider Alumni (Retired)

Posted: ‎2015-01-22 04:38 PM

0 Likes
2
1578
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
‎2015-01-22 04:38 PM

Hi Philippe, you might need to set the nominal voltage for Sag/Swells in order for the meter to capture waveforms. I know this setting impacts a lot of the power quality features. You can do this in the ION Setup Assistant, on the Power Quality > Sag/Swell screen. There should be a setting for nominal voltage.

Reply
Hal_Etheridge
Janeway Hal_Etheridge Janeway
Janeway

Posted: ‎2015-01-22 04:49 PM

0 Likes
0
1578
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
‎2015-01-22 04:49 PM

The nominal voltage setting is required by the Sag/Swell module to correctly trigger waveforms *through that module*.  The nominal voltage should not need to be set to capture waveforms in general.  For instance you can manually trigger a waveform capture without setting this value.  What setting the nominal value does is configuring the Sag/Swell module thresholds as to what is a Sag or Swell.  No setting means no Sag or Swells will be detected and thus no waveforms will be automatically triggered in that particular situation as a side effect.

For the question whether the nominal voltage you need to program is the primary or secondary voltage I am not sure.

Reply
Bojan
Admiral Bojan Admiral
Admiral

Posted: ‎2015-01-23 06:31 AM

0 Likes
0
1579
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
‎2015-01-23 06:31 AM

Hi Christine,

I think Philippe is asking about nominal voltage from Basic Setup, not Sag / Swell Module Settings - Nominal Voltage from Basic Setup is for harmonics calculation, and Nom Volts from Sag / Swell Module Settings is used for all Power Quality functions.

According to ION7650 / 7550 Programming Guide Nom Volts from Sag / Swell Module Settings is the primary power system voltage (sometimes different than PT Primary setup register value), which should be the same as Nominal Voltage from Basic Setup, I guess.

Best Regards,

Bojan

Reply
Preview Exit Preview

never-displayed

You must be signed in to add attachments

never-displayed
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
Create your free account or log in to subscribe to the board - and gain access to more than 10,000+ support articles along with insights from experts and peers.