Our Community ranking system has recently been updated. You may notice changes in user rankings and receive system messages or notifications. If you have questions about how the new ranking works, please refer to the announcement post for more details (click here).

ION7550 Modbus register show wrong data

Metering & Power Quality

Schneider Electric support forum about Power Meters (ION, PowerTag, PowerLogic) and Power Quality from design, implementation to troubleshooting and more.
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
  • ION7550 Modbus register show wrong data
Options
  • Mark Topic as New
  • Mark Topic as Read
  • Float this Topic for Current User
  • Bookmark
  • Subscribe
  • Mute
  • Printer Friendly Page
Invite a Co-worker
Send a co-worker an invite to the portal.Just enter their email address and we'll connect them to register. After joining, they will belong to the same company.
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
581
Mehran_Mehrnia
Mehran_Mehrnia Champion
216
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
Anonymous user
Not applicable

Posted: ‎2017-03-29 03:07 AM

0 Likes
1
1397
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
‎2017-03-29 03:07 AM

ION7550 Modbus register show wrong data

Hi all,

I am reading data from ion 7550 about pc via modbus. But the data read is incorrect.

Read register 40198 is correct.

read register 40200 is correct

read register 40202 is correct

but read register 40204 is wrong.

For more details, open the included file.

Please Help me with this case.

Thanks,

Ta Cong


Attachments
Reply
  • All forum topics
  • Previous Topic
  • Next Topic
Reply 1
Robert_Lee
Robert_Lee Champion
Champion

Posted: ‎2017-03-29 09:52 AM

1 Like
0
1349
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
‎2017-03-29 09:52 AM

Looking at the result, something is only accessing the value as a 16 bit register instead of a 32 bit one.

26944 decimal = 0x6940 as a 16 bit value

551232 decimal = 0x00086940 as a 32 bit value

So either the register is being scaled incorrectly inside the meter's template or the PC is not reading the register correctly and masking off the first register.

I would suggest using some type of program like Modscan or ION Setup to confirm the register contents by reading all of the registers to see how they are being populated.

If register 40204 does indeed contain 0 while register 40205 contains 0x6940, then the problem is within the actual meter and you will need ION Setup communicating using ION protocol to the 7550 to confirm how the scaling of the kW total is being performed.
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
Create your free account or log in to subscribe to the board - and gain access to more than 10,000+ support articles along with insights from experts and peers.