Our Community ranking system has recently been updated. You may notice changes in user rankings and receive system messages or notifications. If you have questions about how the new ranking works, please refer to the announcement post for more details (click here).

ION Frameworks - Will an 7330 or 7350 Framework work in the PM8000?

Metering & Power Quality

Schneider Electric support forum about Power Meters (ION, PowerTag, PowerLogic) and Power Quality from design, implementation to troubleshooting and more.
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
  • ION Frameworks - Will an 7330 or 7350 Framework work in the PM8000?
Options
  • Mark Topic as New
  • Mark Topic as Read
  • Float this Topic for Current User
  • Bookmark
  • Subscribe
  • Mute
  • Printer Friendly Page
Invite a Co-worker
Send a co-worker an invite to the portal.Just enter their email address and we'll connect them to register. After joining, they will belong to the same company.
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
582
Mehran_Mehrnia
Mehran_Mehrnia Champion
217
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
sesa77974_bridg
sesa77974_bridg Explorer
Explorer

Posted: ‎2015-10-21 01:22 PM

0 Likes
4
1776
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
‎2015-10-21 01:22 PM

ION Frameworks - Will an 7330 or 7350 Framework work in the PM8000?

Hi

Will an 7330 or 7350 Framework work in the PM8000?

Suppose a customer typically orders a 7330 with an AA### suffix (P7330A0B0B0M1A0A-AA150). Would Victoria be able to handle the order if it was METSEPM8240-AA150?

Julian White

Tags (5)
  • Tags:
  • 7330
  • 73307350
  • 7350
  • framework
  • pm8000
Reply
  • All forum topics
  • Previous Topic
  • Next Topic

Accepted Solutions
sesa50168
sesa50168 Leader
Leader

Posted: ‎2015-10-21 02:38 PM

0 Likes
0
1734
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
‎2015-10-21 02:38 PM

In general, it depends on the framework.  There are differences in the ION modules between the ION73x0 meters and the PM8000.  For example, I know of one case, that once the function of the AA code was known, it was realized that the desired function already existed in the PM8000.

To respond specifically to the given example, however, the answer is no.  But not because of the AA code, but because the requested meter has a modem, which is not available in the PM8000.  If the customer was willing to accept a separate modem, we could explore the possibility of the PM8000 with an AA code.

See Answer In Context

Reply
Replies 4
Anonymous user
Not applicable

Posted: ‎2015-10-21 01:47 PM

0 Likes
0
1734
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
‎2015-10-21 01:47 PM

I suspect that a new AA code will need to be created for the PM8000. The question should probably be directed to Victoria Order Services (Victoria Order Services EM/Canada/Schneider) for clarification as GSC isn't active on this forum.

Adam

Reply
sesa50168
sesa50168 Leader
Leader

Posted: ‎2015-10-21 02:38 PM

0 Likes
0
1734
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
‎2015-10-21 02:38 PM

In general, it depends on the framework.  There are differences in the ION modules between the ION73x0 meters and the PM8000.  For example, I know of one case, that once the function of the AA code was known, it was realized that the desired function already existed in the PM8000.

To respond specifically to the given example, however, the answer is no.  But not because of the AA code, but because the requested meter has a modem, which is not available in the PM8000.  If the customer was willing to accept a separate modem, we could explore the possibility of the PM8000 with an AA code.

Reply
Robert_Lee
Robert_Lee Champion
Champion

Posted: ‎2015-10-21 02:53 PM

0 Likes
0
1734
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
‎2015-10-21 02:53 PM

Also most of our software isn't designed to allow for cross platform pasting of templates.  It is likely a requirement that the customer would need to submit a new custom PM8000 template which they themselves must provide in order to allow the factory to paste it in.  This might require them to try and paste their previous 73xx framework using ION Designer and resolving any issues themselves and then using ION Setup to upload a new DCF to submit.

Reply
sesa77974_bridg
sesa77974_bridg Explorer
Explorer

Posted: ‎2015-10-21 03:01 PM

0 Likes
0
1734
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
‎2015-10-21 03:01 PM

Thanks everyone
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
Create your free account or log in to subscribe to the board - and gain access to more than 10,000+ support articles along with insights from experts and peers.