Ask our Experts
Didn't find what you are looking for? Ask our experts!
New Community Ranking System
Our Community ranking system has recently been updated. You may notice changes in user rankings and receive system messages or notifications. If you have questions about how the new ranking works, please refer to the announcement post for more details (click here).
Schneider Electric support forum about Power Meters (ION, PowerTag, PowerLogic) and Power Quality from design, implementation to troubleshooting and more.
Search in
Please select a country to continue with beta search.
Link copied. Please paste this link to share this article on your social media post.
This information is available in Vigilohm Catalogue, for each Insulation Monitoring Device.
Search for the "Measurement Voltage" and "Measurement Current" information.
For example:
> for IM400: the injection depends on which Application Mode is setup (Power system, Control command, photovoltaic)
>for XM300
Posted: 2015-06-22 07:51 AM
Link copied. Please paste this link to share this article on your social media post.
For XM300C/XML3xx, there are 2 modes, normal mode with low voltage/current and boost mode with high voltage/current. The IMD changes the mode when Ri cross the alarm threshold. Below is the injection value:
Posted: 2015-10-22 05:01 AM
Link copied. Please paste this link to share this article on your social media post.
For IM400, there are 3 normal mode and 1 boost mode with locating application and when default exist, see diagram below:

in boost mode the IM400 voltage generator is a little more higher(150Vp) and the signal is square 2.5Hz, Below is a shape of the Vf voltage on Rf when IM400 connected with it:
Vfpp=3V Vfp=1.5V
conditions:
IM400 fault threshold = 0.5Kohms, IM400 in locating mode
Rf=400 ohms => IM400 in boost mode with 150Vp scare signal generated
If calculation :
If= Vfp/Rf = 1.5/400 = 0.00375A
this current is closed to the maximum If current (Rf=0) generated by IM400
If max is calculated by 150/40000(Ri) = 0.00375A
You’ve reached the end of your document
Create your free account or log in to subscribe to the board - and gain access to more than 10,000+ support articles along with insights from experts and peers.