Send a co-worker an invite to the Exchange portal.Just enter their email address and we’ll connect them to register. After joining, they will belong to the same company.
Send Invite Cancel
84789members
354238posts

How to integrate a PM710/PM5110/PM850 to a BMS via SNMP?

Metering & Power Quality

Collaborate with multiple experts and discuss various topics about Power Meters and Power Quality. From design & implementation to troubleshooting and more, get support from experts and share your experiences by subscribing to the Schneider Electric Exchange forum today.

Solved
sesa213753
Schneider Alumni (Retired)
Schneider Alumni (Retired)
0 Likes
4
508

How to integrate a PM710/PM5110/PM850 to a BMS via SNMP?

Hi,


One client is trying to read our PM's via SNMP what should be the correct and recommended way to do it ?

Modbus - ? - SNMP


best regards

Tags (4)

Accepted Solutions
waqas_mian
Captain
Captain

Re: How to integrate a PM710/PM5110/PM850 to a BMS via SNMP?

One of my customer wanted the same so i install the following babel buster spx gateway which converts modbus rtu to SNMP

http://www.csimn.com/CSI_pages/BBSPX.html

BR

Genjua

See Answer In Context

4 Replies 4
Yut
Captain
Captain
0 Likes
0
407

Re: How to integrate a PM710/PM5110/PM850 to a BMS via SNMP?

Those meters are using Modbus RTU protocol seems to me that it is impossible to use SNMP, advice your customer to use Modbus RTU.

If there is some particular solution please share.

waqas_mian
Captain
Captain

Re: How to integrate a PM710/PM5110/PM850 to a BMS via SNMP?

One of my customer wanted the same so i install the following babel buster spx gateway which converts modbus rtu to SNMP

http://www.csimn.com/CSI_pages/BBSPX.html

BR

Genjua

sesa213753
Schneider Alumni (Retired)
Schneider Alumni (Retired)
0 Likes
1
408

Re: How to integrate a PM710/PM5110/PM850 to a BMS via SNMP?

Hi Waqas Mian thanks for your recommendation. Just one more thing, i need to install one per meter ? im looking the user guide and i cannot find information about qty of meters per gateway

best regards

waqas_mian
Captain
Captain

Re: How to integrate a PM710/PM5110/PM850 to a BMS via SNMP?

you can connect 32 daisy chain connected Modbus RTU Nodes with a single Babel Buster SPX Gateway.

Following link contain all the information related to gateway.

Modbus to SNMP Gateway: Babel Buster SPX

Also you can have a online demo of the gateway from the following link:

http://csimn.com/DemoWebSPX/\

BR

Genjua

Attachments