Ask our Experts
Didn't find what you are looking for? Ask our experts!
New Community Ranking System
Our Community ranking system has recently been updated. You may notice changes in user rankings and receive system messages or notifications. If you have questions about how the new ranking works, please refer to the announcement post for more details (click here).
Schneider Electric support forum about Power Meters (ION, PowerTag, PowerLogic) and Power Quality from design, implementation to troubleshooting and more.
Search in
Link copied. Please paste this link to share this article on your social media post.
I'd like to know about the max number of ION9000's records.
I think that the max number of the records are below.
・Events:5000
・Historical Alarms:25
・Active Alarms:??
Do you have any idea?
Regards,
Okada
Link copied. Please paste this link to share this article on your social media post.
The Event Log Controller default depth is 5000, but can be user configured to a maximum of 20000. These events can be viewed on the display and/or read over comms with ION protocol.
"Alarms" are not accessible over comms nor web and only viewable on the display interface.
Active Alarms: every possible alarm source has a reserved position. In total, there are up to 148 alarm sources visible on the display only.
Historical Alarms: depth of 25 visible on the display only
Dan
Link copied. Please paste this link to share this article on your social media post.
The Event Log Controller default depth is 5000, but can be user configured to a maximum of 20000. These events can be viewed on the display and/or read over comms with ION protocol.
"Alarms" are not accessible over comms nor web and only viewable on the display interface.
Active Alarms: every possible alarm source has a reserved position. In total, there are up to 148 alarm sources visible on the display only.
Historical Alarms: depth of 25 visible on the display only
Dan
Link copied. Please paste this link to share this article on your social media post.
Link copied. Please paste this link to share this article on your social media post.
The PM8000 has basically the same capabilities in these regards.
The one minor difference is a slightly reduced set of possible simultaneous active alarm sources (ie. fewer digital inputs, no transients, and some reduced module count capabilities)
You’ve reached the end of your document
Create your free account or log in to subscribe to the board - and gain access to more than 10,000+ support articles along with insights from experts and peers.