Our Community ranking system has recently been updated. You may notice changes in user rankings and receive system messages or notifications. If you have questions about how the new ranking works, please refer to the announcement post for more details (click here).

Have you ever wondered how many logs your ION meter can store?

Metering & Power Quality

Schneider Electric support forum about Power Meters (ION, PowerTag, PowerLogic) and Power Quality from design, implementation to troubleshooting and more.
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
  • Have you ever wondered how many logs your ION meter can store?
Options
  • Mark Topic as New
  • Mark Topic as Read
  • Float this Topic for Current User
  • Bookmark
  • Subscribe
  • Mute
  • Printer Friendly Page
Invite a Co-worker
Send a co-worker an invite to the portal.Just enter their email address and we'll connect them to register. After joining, they will belong to the same company.
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
582
Mehran_Mehrnia
Mehran_Mehrnia Champion
216
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
Sanjeet_Sahota
Sanjeet_Sahota Mentor
Mentor

Posted: ‎2020-01-06 04:10 PM

5 Likes
1
2964
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
‎2020-01-06 04:10 PM

Have you ever wondered how many logs your ION meter can store?

With the need to record more data than ever, it can be a challenge to balance the number of logs stored on a device against a fixed memory space and how frequently data is being recorded.   However, with the use of ION technology we have been able to minimize the memory footprint each data log requires to allow for more data to be stored.

With ION meters allowing up to 50 data recorder modules, with 16 inputs each, calculating the amount of space required for logs becomes a necessity to maximize the information needed.  This can also be used to understand how much data is being consumed when communicating over cell modem. This will provide a rough estimate on the amount data that would be required when accessing the meter allowing you to pick the right data plan for your device.

 

 Below outlines how much memory is required to store a single log of data:

Datarecorder Formula.png

 

Using this formula, the amount of memory used by a single data recorder can be calculated under certain conditions. See below for example:

# Channels

Log interval (mins)

Days of Data storage

Depth

kB Used

16

15

120

11520

990

 

Datarecorder Formula FIlled in.png

 

Similarly, Waveform Recorders use the same memory pool as the Data Recorders. You can also calculate the amount of memory required for your Waveform Recorders:

 

Waveform Formula.png

 

 

*Sample Rate & Cycles Per Capture* - This is as configured in the Waveform Recorder as seen in the screenshot below:

 

IONseutp.png

 

Filling in the formula above using the setup from the screenshot above, you can calculate the total capacity to be:

Depth Setting

Sample Rate

Cycles per Capture

kB Used

30

1024

2

122

 

Attached to this post is a basic Excel template that can be used to determine how much memory your current configuration is using.  All cells highlighted in grey can be modified to help calculate your memory usage.  Make the most of your data!

 

Attachments
Memory_and_logging_calculation_tool_spreadsheet_for_ION.xls
Tags (5)
  • Tags:
  • data recorders
  • depth
  • logging
  • memory
  • revenue log
Reply
  • All forum topics
  • Previous Topic
  • Next Topic

Accepted Solutions
Anonymous user
Not applicable

Posted: ‎2020-02-26 09:12 AM

1 Like
0
2932
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
‎2020-02-26 09:12 AM

Hello @Sanjeet_Sahota,

 

Thank you for sharing this useful information with the community. 🙂

 

See Answer In Context

Reply
Reply 1
Anonymous user
Not applicable

Posted: ‎2020-02-26 09:12 AM

1 Like
0
2932
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
‎2020-02-26 09:12 AM

Hello @Sanjeet_Sahota,

 

Thank you for sharing this useful information with the community. 🙂
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
Create your free account or log in to subscribe to the board - and gain access to more than 10,000+ support articles along with insights from experts and peers.