Our Community ranking system has recently been updated. You may notice changes in user rankings and receive system messages or notifications. If you have questions about how the new ranking works, please refer to the announcement post for more details (click here).

HDPM6000 system

Metering & Power Quality

Schneider Electric support forum about Power Meters (ION, PowerTag, PowerLogic) and Power Quality from design, implementation to troubleshooting and more.
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
  • HDPM6000 system
Options
  • Mark Topic as New
  • Mark Topic as Read
  • Float this Topic for Current User
  • Bookmark
  • Subscribe
  • Mute
  • Printer Friendly Page
Invite a Co-worker
Send a co-worker an invite to the portal.Just enter their email address and we'll connect them to register. After joining, they will belong to the same company.
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
582
Mehran_Mehrnia
Mehran_Mehrnia Champion
217
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
BrianW
BrianW
Contributor

Posted: ‎2025-01-09 05:32 AM

0 Likes
1
1265
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
‎2025-01-09 05:32 AM

HDPM6000 system

Hi,

Can anyone offer any assistance with the following issues that we are constantly seeing with installation and testing of HDPM6000 systems?

Normally we are using the 42 channel HDPM6000R interface in IEC channel configuration mode. After the basic commissioning, setting up CT types and channels, etc, we are seeing the following issues:

  • When viewing the various CTs on the associated HMI or with the web interface, the response is extremely laggy, meaning that the screen refresh rate is very slow or sluggish in response, channel information in the various columns appears then disappears, changes in loads take quite a while to correctly display on the HMI, etc.
  • Is there a way to change the colouring of the channel number background, as it can get slightly confusing with the blue background getting confused for a neutral channel especially scrolling down the available listing.

If anyone can suggest methods of getting the information to display in a real time manner, this would be a great benefit.

 

Regards,

Brian

Labels
  • Labels:
  • HDPM6000
Tags (1)
  • Tags:
  • english
Reply
  • All forum topics
  • Previous Topic
  • Next Topic

Accepted Solutions
Mehran_Mehrnia
Mehran_Mehrnia Champion
Champion

Posted: ‎2025-01-09 12:23 PM

0 Likes
0
1235
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
‎2025-01-09 12:23 PM

Hi @BrianW 

 

You did not mention the firmware version of the HMI whether it is V1.0(the old version) or V2.0, which has some improvements.

 

  • Since HMI is communicating over Modbus serial line with HDPM6000, please ensure the baud rate is the fastest one which is by default is 115200. This behavior can be observed for the first time during commissioning when the HMI tries to poll data from all branches. Once the communication is established, the update rate will not be the same as it was the first time.
  • Changing the color is not possible as it is hardcoded. Depending on how and from which angle the user is viewing the HMI, such as at a sharp angle, it can distort how the background colors are perceived and may appear different.

 

Best Regards,

-Mehran

L3 Expert Advanced metering

See Answer In Context

Reply
Reply 1
Mehran_Mehrnia
Mehran_Mehrnia Champion
Champion

Posted: ‎2025-01-09 12:23 PM

0 Likes
0
1235
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
‎2025-01-09 12:23 PM

Hi @BrianW 

 

You did not mention the firmware version of the HMI whether it is V1.0(the old version) or V2.0, which has some improvements.

 

  • Since HMI is communicating over Modbus serial line with HDPM6000, please ensure the baud rate is the fastest one which is by default is 115200. This behavior can be observed for the first time during commissioning when the HMI tries to poll data from all branches. Once the communication is established, the update rate will not be the same as it was the first time.
  • Changing the color is not possible as it is hardcoded. Depending on how and from which angle the user is viewing the HMI, such as at a sharp angle, it can distort how the background colors are perceived and may appear different.

 

Best Regards,

-Mehran

L3 Expert Advanced metering
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
Create your free account or log in to subscribe to the board - and gain access to more than 10,000+ support articles along with insights from experts and peers.