Our Community ranking system has recently been updated. You may notice changes in user rankings and receive system messages or notifications. If you have questions about how the new ranking works, please refer to the announcement post for more details (click here).

Error Ion Set Up 3.0

Metering & Power Quality

Schneider Electric support forum about Power Meters (ION, PowerTag, PowerLogic) and Power Quality from design, implementation to troubleshooting and more.
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
  • Error Ion Set Up 3.0
Options
  • Mark Topic as New
  • Mark Topic as Read
  • Float this Topic for Current User
  • Bookmark
  • Subscribe
  • Mute
  • Printer Friendly Page
Invite a Co-worker
Send a co-worker an invite to the portal.Just enter their email address and we'll connect them to register. After joining, they will belong to the same company.
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
582
Mehran_Mehrnia
Mehran_Mehrnia Champion
217
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
MarthaV
MarthaV
Troubleshooter

Posted: ‎2013-07-22 08:13 AM . Last Modified: ‎2020-04-22 01:55 AM

1 Like
5
2867
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
‎2013-07-22 08:13 AM

Error Ion Set Up 3.0

This error appears when click ¨ok¨ after inserting a new meter.

What is this about?

Attachments
Labels
  • Labels:
  • ION Setup
Tags (1)
  • Tags:
  • ion_setup
Reply
  • All forum topics
  • Previous Topic
  • Next Topic
Replies 5
Matt_Curry
Matt_Curry Champion
Champion

Posted: ‎2013-07-22 09:14 AM

0 Likes
0
2787
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
‎2013-07-22 09:14 AM

Hi Martha,

Welcome to the Solutions Expert Community.  I have moved your post to the ION Setup community so that it will have a better chance of being answered.  If you have any question about the site at all, please let me know.

Cheers,

Matt

Reply
Robert_Lee
Robert_Lee Champion
Champion

Posted: ‎2013-07-22 10:01 AM

1 Like
0
2787
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
‎2013-07-22 10:01 AM

Hi Martha,

     Looking at the error, it seems the installer didn't operate properly as it seems the ION Setup application was installed into a user location for some reason (looking at the error in the dialog the path for the EXE is located in a user sub-folder).

I would recommend uninstalling first and then manually removing any registry keys found in the HKEY_LOCAL_MACHINE\SOFTWARE\SCHNEIDER ELECTRIC\ION Setup location and then attempting to reinstall again.

When installed properly, the application files should reside in the Program Files location (ex. C:\Program Files\Schneider Electric\ION Setup) while writeable files should go into a user-specific folder (ex. C:\Users\XXXXXXX\AppData\Roaming\Schneider Electric\ION Setup).

I'd also recommend you install with a user that has admin privledges.

If you are still having issues, post again or send me an e-mail.

Reply
Digital_Hastak
Digital_Hastak Troubleshooter
Troubleshooter

Posted: ‎2013-08-07 10:51 PM

0 Likes
0
2787
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
‎2013-08-07 10:51 PM

Hi Robert,

I have had a similar issue with Build 12242 and 13080. I am using Win 7 64 bit.

2029

I have uninstalled it once and checked in Registry, but it still came up again in the new clean install?

I have to click Ignore twice and then it will open ION Setup. Then once I sign in as Supervisor and Password, it will give this pop up again.

Any suggestions?

Regards,
Hastak

Reply
Robert_Lee
Robert_Lee Champion
Champion

Posted: ‎2013-08-08 09:19 AM

1 Like
0
2787
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
‎2013-08-08 09:19 AM

Hi Hastak,

     It sounds since you can get to the login dialog, that there is possibly a corrupted DAT file that is still present even after uninstall (this is due to the fact when you uninstall it still leaves any newly created files left behind).  To actually do a complete uninstall, open the registry and find the USERDIR entry in the ION Setup registry location, this will indicate where the DAT files are stored (ex. C:\Users\JoeSmith\AppData\Schneider Electric\ION Setup) and open that location with Explorer.

After the uninstaller has completed, make sure that any files still remaining in that folder are manually deleted and then run the installer again.

If you do find files remain after you uninstall, I'd be interested in seeing these files to see why they are corrupted as I have recently fixed one of the issues which was causing this exact issue.

Reply
Digital_Hastak
Digital_Hastak Troubleshooter
Troubleshooter

Posted: ‎2013-08-08 04:20 PM

0 Likes
0
2787
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
‎2013-08-08 04:20 PM

Thanks for your help Robert.

I checked the directory you mentioned and cleaned up the IONSetup folder in that after the uninstall. But in new install again it gave me same issues and the no. of error pop-up windows actually increased.

And what I noticed as well was my old meter folders and sites still existed. That led me to check the location of Config directory.

2030

So I uninstalled IONSetup again and checked the location of Config Directory and also Program Directory. Deleted the ION Setup folder under both directories completely and VOILA!! it worked. No problems in the new install.

I will put this issue in the local database as well if someone else faces it. However I am not sure if we can implement the clean up of this directory in the UN-INSTALL of ION Setup. I know for Unity Pro, we have a seperate program called Unity Cleaner.

Thanks for your help.

Regards,
Hastak
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
Create your free account or log in to subscribe to the board - and gain access to more than 10,000+ support articles along with insights from experts and peers.