Ask our Experts
Didn't find what you are looking for? Ask our experts!
New Community Ranking System
Our Community ranking system has recently been updated. You may notice changes in user rankings and receive system messages or notifications. If you have questions about how the new ranking works, please refer to the announcement post for more details (click here).
Schneider Electric support forum about Power Meters (ION, PowerTag, PowerLogic) and Power Quality from design, implementation to troubleshooting and more.
Search in
Link copied. Please paste this link to share this article on your social media post.
Energy Meter Evaluation: ION-8650 vs SEL-735
Hi everyone,
We’re in the process of replacing our energy meters and currently evaluating two options: Schneider Electric ION-8650 and SEL-735 from Schweitzer Engineering Laboratories.
I’d like to know:
I’d really appreciate any experiences or recommendations you can share.
Link copied. Please paste this link to share this article on your social media post.
While I can provide features and capabilities of the meter, I cannot definitively say which one is more reliable or prone to operational issues. Reliability can vary depending on the specific application, installation environment, and integration requirements.
It's best to evaluate each option based on your system needs, historical performance data, and support expectations.
Here are some highlighted features of the ION8650 that make it a leading choice for utility metering applications:
| Category | ION-8650 Superiority |
|---|---|
| Sampling Rate | 1024 samples/cycle enables finer resolution for transient and PQ analysis. |
| Modular Architecture | ION™ architecture allows highly customizable logic, data mapping, and control schemes |
| Integration Ecosystem | Seamless integration with Schneider Electric application software such as Power Monitoring Expert (PME), Power Operation (EPO), and others offering end-to-end energy management and advanced analytics. |
| Web Interface & Remote Access | Built-in HTML web server, SFTP, etc. , and ION Setup, more flexible remote configuration and diagnostics. |
| Multi-Protocol Support | Supports Modbus, DNP, DLMS, Itron MV-90, and IEC 61850 Ed. 2, giving broader compatibility with utility and industrial systems. |
| Form Factor Flexibility | Available in socket and switchboard forms, with multiple voltage/current input options for diverse installations. |
| Disturbance & Transient Logging | Advanced sub-cycle disturbance capture and transient detection with high-speed logging. |
| Global Certifications | Extensive compliance with ANSI, IEC, IEEE, EN standards ideal for multinational deployments. |
| Time Synchronization | Supports IRIG-B, SNTP, and GPS time sync for precise event correlation across systems. |
Feedback from other users or field experience may offer additional insights into how each meter performs in real-world conditions.
Best Regards,
-Mehran
L3 Expert Advanced metering
Link copied. Please paste this link to share this article on your social media post.
While I can provide features and capabilities of the meter, I cannot definitively say which one is more reliable or prone to operational issues. Reliability can vary depending on the specific application, installation environment, and integration requirements.
It's best to evaluate each option based on your system needs, historical performance data, and support expectations.
Here are some highlighted features of the ION8650 that make it a leading choice for utility metering applications:
| Category | ION-8650 Superiority |
|---|---|
| Sampling Rate | 1024 samples/cycle enables finer resolution for transient and PQ analysis. |
| Modular Architecture | ION™ architecture allows highly customizable logic, data mapping, and control schemes |
| Integration Ecosystem | Seamless integration with Schneider Electric application software such as Power Monitoring Expert (PME), Power Operation (EPO), and others offering end-to-end energy management and advanced analytics. |
| Web Interface & Remote Access | Built-in HTML web server, SFTP, etc. , and ION Setup, more flexible remote configuration and diagnostics. |
| Multi-Protocol Support | Supports Modbus, DNP, DLMS, Itron MV-90, and IEC 61850 Ed. 2, giving broader compatibility with utility and industrial systems. |
| Form Factor Flexibility | Available in socket and switchboard forms, with multiple voltage/current input options for diverse installations. |
| Disturbance & Transient Logging | Advanced sub-cycle disturbance capture and transient detection with high-speed logging. |
| Global Certifications | Extensive compliance with ANSI, IEC, IEEE, EN standards ideal for multinational deployments. |
| Time Synchronization | Supports IRIG-B, SNTP, and GPS time sync for precise event correlation across systems. |
Feedback from other users or field experience may offer additional insights into how each meter performs in real-world conditions.
Best Regards,
-Mehran
L3 Expert Advanced metering
Link copied. Please paste this link to share this article on your social media post.
We have both. We are almost finished changing our phone line line meters to the ION 8650 meters. These were cheaper than the SEL 735 for meter replacements and did not require changing out the meter base like the SEL 735s would. We do have a few meters installations inside substations and this is where we are using the SEL meters.
Link copied. Please paste this link to share this article on your social media post.
Looking over the SEL-735 myself, seems more straight forward better overall meter if you will be using the extra utility grade SEL integrations or plan to. The 8650's have had bugs where if you turn on demand forgiveness mode the meter stops recording demand entirely, just stays locked at zero. Not sure how 735 work, but any change to an internal logged parameter causes all logged data to be lost on the device. I've had issues with using 8650 meters not using security option 1 I believe (normal hardware lock), the old one, if the nicer templated 8 option is selected (again from memory, like enhanced security I think its called) which is what SE will try to sell it will cause errors in PME every few milliseconds that require wiping the feature rich template out for the more generic one in the other setup. I like to track Delivered and Received registers separately to track PQ issues or unapproved exports, but the modbus map on 8650 requires modification to add Del and Rec for kW, kVAR, and kVA because they only provide net measurements del - rec for those. 735 have considerably more logging capability 1 gig vs 128 max, and by default just use industry standard comtrade and MV-90. I haven't had issues with 8650s, and think the 8650C is a very nice meter for the pricing, especially compared to SE's other low grade options like PM5000s, however all the software to configure it is jank. If you make a custom data log set for the 8650C ION Setup CANNOT see it, nor download the logs, PME seems to be ok logging, but you CANNOT get the data from Ion Setup. You HAVE to make custom profiles for the meter type to manually add those logs so ION Setup can do things with them beyond defining them. If you use the 8650C its default logs are practically useless so you will definitely want to add your own. Not sure how 735 handles this, but working on becoming more informed. Pricing wise not sure why folks say 8650 is cheaper, list pricing on SEL website 735 is better than the pricing I get from Schneider 8650A in form 9S and has much better features, and is a fraction of the meter alone price for an ION 9000 which is the only other meter I know of with 1 gig of logging space. If you are not tied to using PME, I would maybe strongly consider the 735 over the 8650 myself. Also helps it doesn't require a socket, and sockets are getting ridiculously too hard to find with reasonable lead times in my region. If using PME already, maybe there are more things to consider, but even software wise the SEL appears to be cheaper to run than a PME license with advanced meter support which is necessary for IONs. As far as PQ, well that requires the PQ software, and PME 2024R3 won't even see my Ion meters to even look at the PQ data, and PQ takes 8650A to get waveform capture. SE is commercial customers, SEL is utility customers you do the math.
Link copied. Please paste this link to share this article on your social media post.
You get none of those programming ION features without a tool like Designer in PME platform. Sure you can load frameworks with ION Setup, but you'd have to manually code the XML for them to work. As far as I can tell there is no way to program ION without extra bought software. Of course you only lay out the 8650A series when quoting the specs too, so at least +$2000 over the list price of the 735. and IRIG-B has BNC inputs on the 735, the 8650 has none of that. Customized logs are not available for use with Ion Setup unless you manually code them into the profiles for the meter, in a hidden obfuscated and undocumented location in the application data for Ion Setup. the 8650 doesn't seem to be able to provide synchrophasers, display polar symmetric component phasors. it has 1/10 the onboard logging capabilities. 8650 is not technically superior, its a good meter, but the 735 is a strong contender and has many better features. It comes down to how you intend to use the things, and how tied to SE you want to make yourself.
You’ve reached the end of your document
Create your free account or log in to subscribe to the board - and gain access to more than 10,000+ support articles along with insights from experts and peers.