Our Community ranking system has recently been updated. You may notice changes in user rankings and receive system messages or notifications. If you have questions about how the new ranking works, please refer to the announcement post for more details (click here).

Easy Transfer of logging alarm templates between CM4000 meters

Metering & Power Quality

Schneider Electric support forum about Power Meters (ION, PowerTag, PowerLogic) and Power Quality from design, implementation to troubleshooting and more.
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
  • EcoStruxure Power & Grid
  • Metering & Power Quality
  • Re: Easy Transfer of logging alarm templates between CM4000 meters
Options
  • Mark Topic as New
  • Mark Topic as Read
  • Float this Topic for Current User
  • Bookmark
  • Subscribe
  • Mute
  • Printer Friendly Page
Invite a Co-worker
Send a co-worker an invite to the portal.Just enter their email address and we'll connect them to register. After joining, they will belong to the same company.
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
Charles_Murison
Charles_Murison Champion
571
Mehran_Mehrnia
Mehran_Mehrnia Champion
202
Ramasamy_N
Ramasamy_N Champion
115
View All

Recommended Forums

  • SmartConnector Forum

Invite a Colleague

Found this content useful? Share it with a Colleague!

Invite a Colleague Invite
Solved Go to Solution
Back to Metering & Power Quality
Start a Topic
Solved
michael_franz
michael_franz
Mentor

Posted: ‎2017-01-03 12:22 PM

0 Likes
2
1769
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
‎2017-01-03 12:22 PM

Easy Transfer of logging alarm templates between CM4000 meters

TEAM:

We have a site with two dozen CM4000 meters and would like to standardize templates for logging and some alarms.  Will ION Setup help with this?

Sincerely,

Michael

Reply
  • All forum topics
  • Previous Topic
  • Next Topic

Accepted Solutions
Anonymous user
Not applicable

Posted: ‎2017-01-12 11:39 AM

1 Like
0
1735
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
‎2017-01-12 11:39 AM

Yes IONSetup can be used to save the alarms and data logs to be copied from one device to the other.

One thing to be mindful of when performing this is that if the devices basic configuration is configured differently then the alarms may not behave as intended. Basic config is also a selectable parameter when loading in a template.

See Answer In Context

Reply
Replies 2
Yu_Diao
Yu_Diao Leader
Leader

Posted: ‎2017-01-06 01:37 AM

0 Likes
1
1735
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
‎2017-01-06 01:37 AM

ION Setup can save data log and alarm configration into template file and you can reuse it to other CM4s assuming they are exactly the same mode number.

Regards

Reply
Anonymous user
Not applicable

Posted: ‎2017-01-12 11:39 AM

1 Like
0
1736
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
‎2017-01-12 11:39 AM

Yes IONSetup can be used to save the alarms and data logs to be copied from one device to the other.

One thing to be mindful of when performing this is that if the devices basic configuration is configured differently then the alarms may not behave as intended. Basic config is also a selectable parameter when loading in a template.
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
Create your free account or log in to subscribe to the board - and gain access to more than 10,000+ support articles along with insights from experts and peers.