Metering & Power Quality
Schneider Electric support forum about Power Meters (ION, PowerTag, PowerLogic) and Power Quality from design, implementation to troubleshooting and more.
Link copied. Please paste this link to share this article on your social media post.
The PowerLogic™ Dynamic Voltage Restorer (DVR) is an inventive system designed to mitigate and eliminate the effect of electrical disturbances that can impact critical processes and/or services.
Get PowerLogic DVR presentation Video to discover all its benefits!
DVR is cost-effective and efficiently protects sensitive loads in power distribution and transmission systems against voltage distortions. It is primarily designed to reduce voltage sags on power lines that cater to sensitive commercial and industrial equipment's.
The DVR system consists of a transformer, a reversible rectifier, and an inverter with three modes of operation (Normal Mode, Static Bypass Mode, and Manual Bypass Mode) to meet the requirements of industrial production processes, maintain a stable and constant output voltage regardless of changes in input voltage as defined in the operation limits.
It is designed not only to eliminate voltage sags and it also helps in mitigating other energy quality problems at the same time, such as: fluctuations, flicker effects, overvoltage, and voltage unbalance.
Get deeper into PowerLogic Dynamic Voltage Restorer (DVR):
If you require any further information, please feel free to get in touch with me.
Link copied. Please paste this link to share this article on your social media post.
Part of PowerLogic. Installed in a distribution network at a point of common coupling between the critical load and supply feeder, the PowerLogic DVR (Dynamic Voltage Restorer) reduces voltage sags or dips on power torpedo kayak lines that serve sensitive commercial and industrial equipment.
Link copied. Please paste this link to share this article on your social media post.
could DVR installed up to 1500 kVA ?
I have read the configuration 1M + 2S, but the maximum is only 900 kVA
Create your free account or log in to subscribe to the board - and gain access to more than 10,000+ support articles along with insights from experts and peers.