Our Community ranking system has recently been updated. You may notice changes in user rankings and receive system messages or notifications. If you have questions about how the new ranking works, please refer to the announcement post for more details (click here).

Tesla EV charger load management CTs don't fit Square D SC3042M200PF meter panel bus bars

Metering & Power Quality

Schneider Electric support forum about Power Meters (ION, PowerTag, PowerLogic) and Power Quality from design, implementation to troubleshooting and more.
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
  • Tesla EV charger load management CTs don't fit Square D SC3042M200PF meter panel bus bars
Options
  • Mark Topic as New
  • Mark Topic as Read
  • Float this Topic for Current User
  • Bookmark
  • Subscribe
  • Mute
  • Printer Friendly Page
Invite a Co-worker
Send a co-worker an invite to the portal.Just enter their email address and we'll connect them to register. After joining, they will belong to the same company.
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
582
Mehran_Mehrnia
Mehran_Mehrnia Champion
216
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
jcbottorff
jcbottorff
Explorer

Posted: ‎2024-03-05 10:57 PM

0 Likes
4
4385
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
‎2024-03-05 10:57 PM

Tesla EV charger load management CTs don't fit Square D SC3042M200PF meter panel bus bars

I'm installing a Tesla Wall Connector EV charger using the Tesla dynamic load management controller (Neurio device).  The EV charger talks to the load controller over a RS-485 twisted pair using the modbus protocol. This allows setting the EV charger to deliver up to a full 48A, but reduce it if needed to assure the panel input current never exceeds 160A continuously (200A main breaker, panel has 225A bus). The existing maximum load calculation does not have an extra 48A required for permit approval. The split CT clamps (photo below) they supply don't quite close when put on the bus bars, there is a 1/8" gap. The CTs say they work up to a wire diameter of 0.75", but apparently the rectangular bus bars exceed this. I'm assuming split CT's don't work correctly unless the split gap is fully closed. The CTs for the Enphase solar system fit just fine, which must have about a 1" square hole. The original plan was to put the Tesla CTs above the already installed Enphase CTs, which I read works fine as long as I leave a 1" gap (as per info from a CT manufacturer).

 

This panel model is quite popular for people doing solar installs. Using a load controller like this seems like a better strategy than degrading the charging rate or what in many cases would be a very expensive service upgrade.

 

I haven't seen any evidence Tesla has alternative CTs with a bigger hole so am wondering if I could put the CTs before the meter around the incoming utility cables, which are round and am pretty sure would fit. This section of the meter panel has a utility company seal (left of meter in below photo), so assume I would have to get the power company to at least come inspect the CTs and put a new seal on the meter upstream compartment, if they even allow CTs to be placed before the meter. It's unclear if there are any holes from this section of the panel into an an adjoining customer accessible section, so might have to drill a small hole and put a rubber grommet for the CT wires to come through. This is PG&E in northern California.  

 

Attachments
Tags (1)
  • Tags:
  • english
Reply
  • All forum topics
  • Previous Topic
  • Next Topic

Accepted Solutions
Ramasamy_N
Ramasamy_N Champion
Champion

Posted: ‎2024-12-20 04:15 AM

1 Like
0
3775
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
‎2024-12-20 04:15 AM

Please connect with the respective technical support team. 

See Answer In Context

Reply
Replies 4
Ramasamy_N
Ramasamy_N Champion
Champion

Posted: ‎2024-12-20 04:15 AM

1 Like
0
3775
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
‎2024-12-20 04:15 AM

Please connect with the respective technical support team. 

Reply
EnlightenedElectrical
EnlightenedElectrical
Explorer

Posted: ‎2025-07-12 02:03 PM

0 Likes
2
3064
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
‎2025-07-12 02:03 PM

Hello can you please share the model number of the Tesla NEURIO dynamic Power meter? Is it Tesla 1112484-99-A or possibly Neurio meter 1938241-00-A. Tesla sent me the 1938241-00-A version and Tesla One app does not see it. Im trying to get it working with Tesla Gen 3 Wall Connector in USA. Thanks. 

Reply
Charles_Murison
Charles_Murison Champion
Champion

Posted: ‎2025-07-14 08:55 AM

0 Likes
0
3063
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
‎2025-07-14 08:55 AM

Hello @EnlightenedElectrical ,

I would recommend reaching out to Tesla support for a Tesla product.

 

Regards,

Charles

L4 Prime for Advanced metering and Utilities
Reply
jcbottorff
jcbottorff
Explorer

Posted: ‎2025-07-15 01:21 AM

0 Likes
0
3051
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
‎2025-07-15 01:21 AM

That's exactly the part number I received. If it does not show up in the Tesla One app that suggests it's not working. You do need to feed it power on the voltage legs to run the internal electronics. It believe it will not show up unless the wall charger detects it it responds. The wall controller will be sending modbus reads every second or so. If it doesn't work try flipping the +/- RS-485 signals, there labeling as I remember is not so clear.
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
Create your free account or log in to subscribe to the board - and gain access to more than 10,000+ support articles along with insights from experts and peers.