Our Community ranking system has recently been updated. You may notice changes in user rankings and receive system messages or notifications. If you have questions about how the new ranking works, please refer to the announcement post for more details (click here).

Connect PM1000 to PME2021

Metering & Power Quality

Schneider Electric support forum about Power Meters (ION, PowerTag, PowerLogic) and Power Quality from design, implementation to troubleshooting and more.
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
  • EcoStruxure Power & Grid
  • Metering & Power Quality
  • Connect PM1000 to PME2021
Options
  • Mark Topic as New
  • Mark Topic as Read
  • Float this Topic for Current User
  • Bookmark
  • Subscribe
  • Mute
  • Printer Friendly Page
Invite a Co-worker
Send a co-worker an invite to the portal.Just enter their email address and we'll connect them to register. After joining, they will belong to the same company.
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
Charles_Murison
Charles_Murison Champion
566
Mehran_Mehrnia
Mehran_Mehrnia Champion
194
Ramasamy_N
Ramasamy_N Champion
115
View All

Recommended Forums

  • SmartConnector Forum

Invite a Colleague

Found this content useful? Share it with a Colleague!

Invite a Colleague Invite
Solved Go to Solution
Back to Metering & Power Quality
Start a Topic
Solved
SESA528
SESA528 Contributor
Contributor

Posted: ‎2022-03-30 10:52 AM

0 Likes
1
2265
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
‎2022-03-30 10:52 AM

Connect PM1000 to PME2021

Hi admin,

 

My customer have PM1000. I saw PM1000 have port communication RS485 (Pin 7_[ D1+] and Pin 14_[D0-] in attached image). But when i connect to PME2021, i can't read data. Pls help me.

 

Thanks very much.

 

IMG_4124.JPGIMG_4133.JPG

Labels
  • Labels:
  • PM Downloads
Tags (1)
  • Tags:
  • english
Reply
  • All forum topics
  • Previous Topic
  • Next Topic

Accepted Solutions
Robert_Lee
Robert_Lee Champion
Champion

Posted: ‎2022-04-05 09:49 AM . Last Modified: ‎2022-04-05 02:22 PM

0 Likes
0
2180
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
‎2022-04-05 09:49 AM

In most cases, to connect a serial device (RS-485) to PME (or any PC-based software), unless the device is within physical proximity to the device *or* existing RS-485 wiring is available (to a maximum of 5000 ft I believe), then the best option is to use some type of Modbus TCP gateway device (like EGX-150/Link 150) that allows a PC to use network TCP Modbus which can then be wired to RS-485 devices.

Usually those devices have a web interface that allows you to properly configure the RS-485 port on the gateway to match up with the settings programmed in any device to allow proper communications.

[Edit]

Upon further investigation, the PM1000 does not come with standard Modbus communications (only a DO which can be used for energy pulsing).  The PM1200 is the one that has RS-485 communications (see attached differences between the two models).

https://www.se.com/ww/en/product-range/7206-easylogic-pm1000-series/#overview

 

See Answer In Context

Attachments
Tags (1)
  • Tags:
  • english
Reply
Reply 1
Robert_Lee
Robert_Lee Champion
Champion

Posted: ‎2022-04-05 09:49 AM . Last Modified: ‎2022-04-05 02:22 PM

0 Likes
0
2181
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
‎2022-04-05 09:49 AM

In most cases, to connect a serial device (RS-485) to PME (or any PC-based software), unless the device is within physical proximity to the device *or* existing RS-485 wiring is available (to a maximum of 5000 ft I believe), then the best option is to use some type of Modbus TCP gateway device (like EGX-150/Link 150) that allows a PC to use network TCP Modbus which can then be wired to RS-485 devices.

Usually those devices have a web interface that allows you to properly configure the RS-485 port on the gateway to match up with the settings programmed in any device to allow proper communications.

[Edit]

Upon further investigation, the PM1000 does not come with standard Modbus communications (only a DO which can be used for energy pulsing).  The PM1200 is the one that has RS-485 communications (see attached differences between the two models).

https://www.se.com/ww/en/product-range/7206-easylogic-pm1000-series/#overview

 
Attachments
Tags (1)
  • Tags:
  • english
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
Create your free account or log in to subscribe to the board - and gain access to more than 10,000+ support articles along with insights from experts and peers.