Our Community ranking system has recently been updated. You may notice changes in user rankings and receive system messages or notifications. If you have questions about how the new ranking works, please refer to the announcement post for more details (click here).

Communikation Problems with EGX100 and SIM10M

Metering & Power Quality

Schneider Electric support forum about Power Meters (ION, PowerTag, PowerLogic) and Power Quality from design, implementation to troubleshooting and more.
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
  • EcoStruxure Power & Grid
  • Metering & Power Quality
  • Communikation Problems with EGX100 and SIM10M
Options
  • Mark Topic as New
  • Mark Topic as Read
  • Float this Topic for Current User
  • Bookmark
  • Subscribe
  • Mute
  • Printer Friendly Page
Invite a Co-worker
Send a co-worker an invite to the portal.Just enter their email address and we'll connect them to register. After joining, they will belong to the same company.
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
Charles_Murison
Charles_Murison Champion
566
Mehran_Mehrnia
Mehran_Mehrnia Champion
194
Ramasamy_N
Ramasamy_N Champion
115
View All

Recommended Forums

  • SmartConnector Forum

Invite a Colleague

Found this content useful? Share it with a Colleague!

Invite a Colleague Invite
Back to Metering & Power Quality
Start a Topic
Sven_Ortmann
Sven_Ortmann Leader
Leader

Posted: ‎2015-11-17 03:39 AM

0 Likes
1
1024
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
‎2015-11-17 03:39 AM

Communikation Problems with EGX100 and SIM10M

Hi,

I want to implement analoge Inputs with the help of SIM10M and EGX100 into PME.

The cabeling is the same way it is described in the install Manual:

Dips of EGX100:

1= OFF

2,3,4,5= ON

Dips of SIM10M:

1= ON (because for testing only one device is connceted)

2,3,4=OFF

Cabeling:

D0 -> RX-

D1-> RX+

I also tested different Settings without luck.

SIM10M is configured with USB and Slave Adresse is set to 1 (all other Settings are Standard)  -> LED Switch from Orange to Green

SIM10M Baud: 19200, Parity: Even Stopbit:1

EGX100: Baud: 19200, Parity: Even, Mode Master, RS485.2wire, Responsetime 3 sec

I want to read the Registers in Webpage of EGX100 but there is always a timeout 😞

What could be wring at this configuration?

EGX100 Firmware: 3.000

SIM10 Firmware: 1.2.0

Thank you

Reply
  • All forum topics
  • Previous Topic
  • Next Topic
Reply 1
michael_franz
michael_franz
Mentor

Posted: ‎2017-06-30 11:40 AM

0 Likes
0
992
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
‎2017-06-30 11:40 AM

Sven:

Is this a new EGX or is it a repurposed unit from an old PowerLogic job?  Check that the web page under devices is set to the correct protocol.  An address can be set to PowerLogic, Modbus or JBus.  If it was on a string with older equipment it may be set to something other than what you need.  Long shot but worth a look.

Michael
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
Create your free account or log in to subscribe to the board - and gain access to more than 10,000+ support articles along with insights from experts and peers.