Our Community ranking system has recently been updated. You may notice changes in user rankings and receive system messages or notifications. If you have questions about how the new ranking works, please refer to the announcement post for more details (click here).

Cannot connect to HDPM6000 after erroneously setting subnet mask 255.255.255.255

Metering & Power Quality

Schneider Electric support forum about Power Meters (ION, PowerTag, PowerLogic) and Power Quality from design, implementation to troubleshooting and more.
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
  • Cannot connect to HDPM6000 after erroneously setting subnet mask 255.255.255.255
Options
  • Mark Topic as New
  • Mark Topic as Read
  • Float this Topic for Current User
  • Bookmark
  • Subscribe
  • Mute
  • Printer Friendly Page
Invite a Co-worker
Send a co-worker an invite to the portal.Just enter their email address and we'll connect them to register. After joining, they will belong to the same company.
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
582
Mehran_Mehrnia
Mehran_Mehrnia Champion
217
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
rcamacker
rcamacker Contributor
Contributor

Posted: ‎2025-02-26 10:46 AM

0 Likes
4
2153
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
‎2025-02-26 10:46 AM

Cannot connect to HDPM6000 after erroneously setting subnet mask 255.255.255.255

Commissioning new HDPM6000. Updated firmware. Set client's requested IP but typo'ed 255.255.255.255 as the subnet mask. Cannot ping, open webpage, Modbus will not connect, no HDPM6000 Manager access. NetCfg can read the address but cannot change it as the firmware of the meter is too new.

Is there any way to change the submask remotely or otherwise connect to the meter?

Labels
  • Labels:
  • HDPM6000
Reply
  • All forum topics
  • Previous Topic
  • Next Topic

Accepted Solutions
rcamacker
rcamacker Contributor
Contributor

Posted: ‎2025-02-26 07:43 PM

0 Likes
1
2132
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
‎2025-02-26 07:43 PM

Thanks for the reply Mehran. Once I had erroneously changed the subnet mask to 255.255.255.255 there was no way to locally connect to the meter. Nothing worked, except NetCfg. However NetCfg could not change the IP address as this firmware was up-graded on the HDPM6000 (After a certain framework NetCfg cannot change the IP address). Had to join the site network to open the webpage.

See Answer In Context

Reply
Replies 4
Mehran_Mehrnia
Mehran_Mehrnia Champion
Champion

Posted: ‎2025-02-26 12:43 PM

2 Likes
0
2142
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
‎2025-02-26 12:43 PM

Hi @rcamacker 

 

The subnet mask of 255.255.255.255 likely has isolated the device from all other devices on the network.

Here are some steps that could help to resolve it:

1- If possible, connect your laptop directly to the meter using an Ethernet cable and assign a static IP address to your computer that is in the same subnet as the meter’s original configuration.

For example, if the meter was previously set to 192.168.1.x, set your computer to 192.168.1.10 and try to connect.

 

2- You mentioned 'Modbus will not connect' and I assume via Modbus TCP, but have you tried connecting serially to the device via a gateway or USB/Serial converter to read the Modbus registers from 4481 using any Modbus application to read the configured/saved IP address and subnet mask of this meter and try to edit them accordingly? 

In this example, I connected through Modbus(in my case via TCP) and wrote the values 255,255,0,0 to the registers 4489-4491:

Mehran_Mehrnia_0-1740602119596.png 

Mehran_Mehrnia_1-1740602255793.png

By default serial Modbus settings of HDPM6000 is as below:
Modbus Slave Address: 1
Baud rate: 115200
Parity: None

 

Best Regards,

-Mehran

L3 Expert Advanced metering

Reply
rcamacker
rcamacker Contributor
Contributor

Posted: ‎2025-02-26 07:43 PM

0 Likes
1
2132
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
‎2025-02-26 07:43 PM

Thanks for the reply Mehran. Once I had erroneously changed the subnet mask to 255.255.255.255 there was no way to locally connect to the meter. Nothing worked, except NetCfg. However NetCfg could not change the IP address as this firmware was up-graded on the HDPM6000 (After a certain framework NetCfg cannot change the IP address). Had to join the site network to open the webpage.

Reply
Charles_Murison
Charles_Murison Champion
Champion

Posted: ‎2025-02-27 11:05 AM

0 Likes
0
2102
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
‎2025-02-27 11:05 AM

Hello @rcamacker ,

Likely when you connected the meter to the network, the meter was able to route traffic through the gateway address.

 

regards,

Charles

L4 Prime for Advanced metering and Utilities
Reply
MeganSteele2024
MeganSteele2024 Explorer
Explorer

Posted: ‎2025-07-01 12:15 PM

0 Likes
0
1575
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
‎2025-07-01 12:15 PM

I am having an issue where I know the IP address because I have a screen capture. It is still default with no changes. I cannot ping or reach the HDPM6000. Any recommendations?
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
Create your free account or log in to subscribe to the board - and gain access to more than 10,000+ support articles along with insights from experts and peers.