Schneider Electric support forum about Power Meters (ION, PowerTag, PowerLogic) and Power Quality from design, implementation to troubleshooting and more.
Send a co-worker an invite to the portal.Just enter their email address and we'll connect them to register. After joining, they will belong to the same company.
You have entered an invalid email address. Please re-enter the email address.
This co-worker has already been invited to the Exchange portal. Please invite another co-worker.
Please enter email address
Send InviteCancel
Invitation Sent
Your invitation was sent.Thanks for sharing Exchange with your co-worker.
Link copied. Please paste this link to share this article on your social media post.
2018-02-2511:44 PM
BCPM 250A branch Split-Core CT
Hi Everyone,
I have a question about BCPM split-core type CT amp ratings.
I have a project that has many 250A branch circuits. BCPMSC E-type meters would be suitable for a few of their panels . Except that according to the BCPM datasheet, split core branch CTs are only available up to 200A. However the specifications for the split-core branch CT and split-core main auxiliary CT seem to be the same - 0.333V output.
BCPMSCCT3 200A split-core 1.8m lead
LVCT00302S 300A split-core 0.333V output
Thus, my question is, can I use the 300A split-core CT (LVCT00302S) on my BCPM branch circuits?