Our Community ranking system has recently been updated. You may notice changes in user rankings and receive system messages or notifications. If you have questions about how the new ranking works, please refer to the announcement post for more details (click here).

BACnet IP server communication failure

Metering & Power Quality

Schneider Electric support forum about Power Meters (ION, PowerTag, PowerLogic) and Power Quality from design, implementation to troubleshooting and more.
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
  • BACnet IP server communication failure
Options
  • Mark Topic as New
  • Mark Topic as Read
  • Float this Topic for Current User
  • Bookmark
  • Subscribe
  • Mute
  • Printer Friendly Page
Invite a Co-worker
Send a co-worker an invite to the portal.Just enter their email address and we'll connect them to register. After joining, they will belong to the same company.
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
582
Mehran_Mehrnia
Mehran_Mehrnia Champion
216
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
KlaudiaKl
KlaudiaKl
Explorer

Posted: ‎2022-03-23 05:04 AM . Last Modified: ‎2022-03-23 05:20 AM

0 Likes
2
4797
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
‎2022-03-23 05:04 AM

BACnet IP server communication failure

Hello!
I've got the issue with communicating Enterprise Server or Automation Server with BACnet IP server gateway (Modbus to BACnet IP Intesis: https://www.intesis.com/products/protocol-translator/modbus-gateways/modbus-rtu-tcp-bac-ibox-bac-mbm). I see it in the device discovery tab as an "Unconfigured Devices" (photo) and I can move the device to the system tree and see the properties, the name of device, the addres etc. but I can't see any variables and I cannot add them manually. We tested the gateway and it communicated with the room unit without problems - we added the registers, we tested read/write functions and it worked (we could change the setpoints, operation mode etc.). The only option I considered was that the gateway have the password and we can't delete it from the device. We entered that password in Workstation Building Operation (version 1.9) but the error "Reject unrecognized service" appeared. Is there other option to add the device and collect the variables from it?

276069710_952298888820578_5651180310290639705_n.jpg

Klaudia

 

Tags (5)
  • Tags:
  • automation server
  • bacnet ip
  • ecostruxure
  • english
  • Enterprise Server.Automation Server.BACnet IP.Modbus.1.9
Reply
  • All forum topics
  • Previous Topic
  • Next Topic

Accepted Solutions
markb_ci3
markb_ci3
Contributor

Posted: ‎2022-03-24 06:17 AM

1 Like
1
4760
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
‎2022-03-24 06:17 AM

Devices that come in as "Unconfigured" usually have a problem with compliance to the BACnet standard.

 

Items that must be unique:

BACnet Address (applies to MSTP)

BACnet Name (workarounds to this are available)

BACnet Device Instance

 

That last one is a deal breaker. BACnet communications won't work if multiple devices are responding to the same ID.

 

There can also be problems with how the device is responding to the "WhoIs" request from the AS-P.

 

Insert a managed switch with a mirrored port in line with the device and do a WireShark capture to see the packets.

 

A "Who-Is" must be followed by an "I-am" by the device and it will provide the device details to the AS-P such as manufacturer, and the read/write properties it supports. If this communication does not happen properly, the AS-P won't know what to do with the device.

 

Armed with a BACnet capture, you should engage the manufacturer to see if they can help.

 

Good luck!

Mark

See Answer In Context

Tags (1)
  • Tags:
  • english
Reply
Replies 2
markb_ci3
markb_ci3
Contributor

Posted: ‎2022-03-24 06:17 AM

1 Like
1
4760
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
‎2022-03-24 06:17 AM

Devices that come in as "Unconfigured" usually have a problem with compliance to the BACnet standard.

 

Items that must be unique:

BACnet Address (applies to MSTP)

BACnet Name (workarounds to this are available)

BACnet Device Instance

 

That last one is a deal breaker. BACnet communications won't work if multiple devices are responding to the same ID.

 

There can also be problems with how the device is responding to the "WhoIs" request from the AS-P.

 

Insert a managed switch with a mirrored port in line with the device and do a WireShark capture to see the packets.

 

A "Who-Is" must be followed by an "I-am" by the device and it will provide the device details to the AS-P such as manufacturer, and the read/write properties it supports. If this communication does not happen properly, the AS-P won't know what to do with the device.

 

Armed with a BACnet capture, you should engage the manufacturer to see if they can help.

 

Good luck!

Mark

Tags (1)
  • Tags:
  • english
Reply
KlaudiaKl
KlaudiaKl
Explorer

Posted: ‎2022-03-29 11:30 AM

0 Likes
0
4701
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
‎2022-03-29 11:30 AM

Hello!
Thank you so much for your reply. We found out that it was the problem with BACnet Device Instance number and with the connection to the internal network. Now we see the device as configured in the Workstation and we can read the values of the units registers. But we got another problem now - we can read the values of the input registers but we can't write data to the outputs - we can't control the unit. When we put for example value of the setpoint of temperature we got the validation error. Maybe it is a problem that the device have the password that can't be delete? Do you got any ideas what we could do to make it work well?

Best Regards,
Klaudia

Tags (1)
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
Create your free account or log in to subscribe to the board - and gain access to more than 10,000+ support articles along with insights from experts and peers.